Programming the Flash gives Sector Protection Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Programming the Flash gives Sector Protection Error

跳至解决方案
2,016 次查看
ramkrishnan
Contributor III

We have a board with the P1022 processor and we had a Cypress (formerly spansion) chip S29GL01GP11TFIR1 for the flash. But that has been obsoleted now and we had to replace it with S29GL01GT10TF1010 chip. 

When we trying put the u-boot.bin file using codewarrior we get the following error. 

Error: Program with Verify failed. Flash driver reports the following error(s): Sector Protection Error
Error: Program with Verify failed. Flash driver reports the following error(s): Sector Protection Error

 

One thing we do see is that the only device listed under "Add Device" is S29GL01GP (We also tried the S29GL01GP-Simics, but for our case 64Mx16X2 it is the same in both the xml files which is amd16x2.elf) , we do not see a S29GL01GT. 

Is there an elf file for this chip ? 

 

The erase, dump (read operation) all seems to work fine and goes thru sucessfully. 

 

I have also attached the Diagnose for both the old flash(S29GL01GP11TFIR1) and the new flash(S29GL01GT10TF1010) and attached it. 

 

Please let me know if you need any more information. 

 

Thank you

Ram Krishnan

Original Attachment has been moved to: OldFlashDiagnose.zip

Original Attachment has been moved to: NewFlashDiagnose.zip

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,691 次查看
ufedor
NXP Employee
NXP Employee

Please create a Technical Case for the in-depth issue investigation:

https://community.freescale.com/thread/381898

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,691 次查看
ramkrishnan
Contributor III

NXP was very helpful in getting this fixed. The solution was a new elf file for the new chip set. The new one seems to work on the older one too.

Thank you,

Ram Krishnan

0 项奖励
回复
1,692 次查看
ufedor
NXP Employee
NXP Employee

Please create a Technical Case for the in-depth issue investigation:

https://community.freescale.com/thread/381898

0 项奖励
回复