I downloaded the virtual box for QorIQ-SDK-V1.8-20150619-yocto
I have not installed anything in addition to what comes with the downloaded virtual image.
I have logged into the virtual box (Not as root) and run:
source ./poky/fsl-setup-poky -m p4080ds
from: :~/SDK/QorIQ-SDK-V1.8-20150619-yocto
I observed that directory "build_p4080ds_release" was created.
if I cd to that directory and run:
source SOURCE_THIS
and
bitbake fsl-image-minimal
... I get the following error:
$ bitbake fsl-image-minimal
ERROR: Traceback (most recent call last):
File "/home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/poky/bitbake/lib/bb/cookerdata.py", line 163, in wrapped
return func(fn, *args)
File "/home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/poky/bitbake/lib/bb/cookerdata.py", line 173, in parse_config_file
return bb.parse.handle(fn, data, include)
File "/home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/poky/bitbake/lib/bb/parse/__init__.py", line 99, in handle
return h['handle'](fn, data, include)
File "/home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/poky/bitbake/lib/bb/parse/parse_py/ConfHandler.py", line 151, in handle
statements.eval(data)
File "/home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/poky/bitbake/lib/bb/parse/ast.py", line 39, in eval
statement.eval(data)
File "/home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/poky/bitbake/lib/bb/parse/ast.py", line 63, in eval
bb.parse.ConfHandler.include(self.filename, s, self.lineno, data, False)
File "/home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/poky/bitbake/lib/bb/parse/parse_py/ConfHandler.py", line 97, in include
ret = handle(fn, data, True)
File "/home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/poky/bitbake/lib/bb/parse/__init__.py", line 99, in handle
return h['handle'](fn, data, include)
File "/home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/poky/bitbake/lib/bb/parse/parse_py/ConfHandler.py", line 147, in handle
feeder(lineno, s, abs_fn, statements)
File "/home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/poky/bitbake/lib/bb/parse/parse_py/ConfHandler.py", line 184, in feeder
raise ParseError("unparsed line: '%s'" % s, fn, lineno);
ParseError: ParseError at /home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/meta-fsl-ppc/conf/machine/p4080ds.conf:1: unparsed line: '#@TYPE: Machine'
ERROR: Unable to parse conf/bitbake.conf: ParseError at /home/freescale/SDK/QorIQ-SDK-V1.8-20150619-yocto/meta-fsl-ppc/conf/machine/p4080ds.conf:1: unparsed line: '#@TYPE: Machine'
freescale@freescale-sdk:~/SDK/QorIQ-SDK-V1.8-20150619-yocto/build_p4080ds_release$
...I am confused. The script finds the proper file (p4080ds.conf) but fails to notice that the first line is commented (?) - or am I supposed to change that line with
UBOOT_MACHINES ?= "P4080DS"
(Which appears further down the script)???
b
Look at attached file.
Use recommended command sequence for VirtualBox using for the QorIQ SDK.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
...Yes, I saw the VM User manual and followed everything religiously.
There is nothing in there that affects this issue.
The VM was installed correctly with the recommended version of Oracle VM Virtual Box (4.3.28)
(And extensions)
The instructions in "QorIQ SDK v1.8 Info Center.pdf" were also followed verbatim.
According to this documentation, I prepared the host environment (page 170) correctly.
I followed all of the instruction up to page 170 (builds)..
where I tried to build a fsl-image-minimal... witht he result posted above....
The bitbake scripts find the p4080ds.conf file, but fail to parser it correctly.
I followed the instructions... It appears that the default virtual image provided does no work.
Please help.
VR,
Bruce
Look at attached file. Do you use similar command sequence?
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I deleted the entire virtual machine and started again (from the same compressed image)
Using the same commands (I copy/pasted them from the same list as the first time)
I am now able to compile correctly and create images.
Thank you for the help. I do not understand what was special about a second install, or what may have been done incorrectly the first time - I'm just glad the images are compiling.
Thank You.
Bruce