PCI: Cannot allocate resource region of root device on P5020 board with stock 3.19-rc2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCI: Cannot allocate resource region of root device on P5020 board with stock 3.19-rc2

1,964 Views
RabbitHoleComp
Contributor II

@Scott Wood, as requested, a new thread for my PCI issues

I've got a heavily-patched version of 3.18.13 that works great on a custom P5020-based ATX board. When I boot 3.19-rc2, I get the following

PCI: Cannot allocate resource region 0 of device 0000:00:00.0, will remap

PCI: Cannot allocate resource region 0 of device 0001:00:00.0, will remap

PCI: Cannot allocate resource region 6 of device 0001:08:00.0, will remap

pci 0000:00:00.0: BAR 0: no space for [mem size 0x01000000]

pci 0000:00:00.0: BAR 0: failed to assign [mem size 0x01000000]

pci 0000:01:00.0: BAR 6: assigned [mem 0xc10040000-0xc1005ffff pref]

Are there any patchsets you can point me at which may not be upstream yet, that would resolve this issue?

Full kernel boot output with 3.19-rc2 at http://pastie.org/private/njlwhfkzulkmy6cau1i8ig

my kernel .config is at http://www.alexperez.com/Cyrus-P5020-3.19-rc2-config.txt

Labels (1)
0 Kudos
5 Replies

876 Views
RabbitHoleComp
Contributor II

Anyone? I am still having no success with PCIe on 3.19-rc6.

0 Kudos

876 Views
scottwood
NXP Employee
NXP Employee

Sorry for the delay.  Could you elaborate on what fails to work with PCIe?  I see similar messages but PCIe devices still work.  The "will remap" lines are not errors -- they are expected in the case where firmware didn't set up usable mappings.  As for BAR 0 of 00:00.0, that's always bit a bit weird on Freescale PCI controllers.  Other devices seem to have their BARs assigned OK from the log.

What is the output of "lspci -v" after booting?

0 Kudos

876 Views
RabbitHoleComp
Contributor II

scottwood, lspci -v shows zero output. There is not even a root device. Kernels up to and including 3.19-rc7 (released yesterday) do not seem to include functional PCI or SATA. I think there's some backsliding going on with regards to upstream support for SATA as well, as it works in 3.18.5, but not in 3.19-rcX

0 Kudos

876 Views
RabbitHoleComp
Contributor II

scottwood This is still a problem with the final release of 3.19.  As an aside, the on-board SATA does not work with 3.19 either, but worked fine in 3.18, so we have a regression on that front. With kernel 3.18.1, lspci -v also shows no output. PCI worked in 3.17.

0 Kudos

876 Views
scottwood
NXP Employee
NXP Employee

SATA and PCI work for me on p5020ds with 3.19.  I suggest bisecting to find the patch that broke these on your board.

0 Kudos