P4080DS reflector is not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080DS reflector is not working

2,762 Views
ankur
Contributor I

Hi,

I am new to Freescale so my questions might be very basic

1. How to identify the revision of P4080DS board?

    My u-boot prints "CPU0:  P4080E, Version: 3.0" in the very startup, is this the revision?

2. as per the SDK fm1-gb1 port is used for Linux kernel which is on the main board, I am not able to ping through this port even the ifconfig shows it is RUNNING, port has RED led

    contantly.

3. I do not have any XAUI card so I programmed SerDes 0x10 RCW rcw_5g_1500mhz.bin, uboot, fman to the flash and boot from bank4, I loaded fsl-image-core and trying sample

    application reflector but it is giving following error

ERR : Invocation of FM_PORT_Open for fm1/port/1G/3 failed

ERR : Invocation of FM_PCD_Disable for fm0/pcd failed with error code 0x00010028

Found /fsl,dpaa/dpa-fman0-oh@1, Tx Channel = 46, FMAN = 0, Port ID = 1

Found /fsl,dpaa/ethernet@5, Tx Channel = 61, FMAN = 1, Port ID = 0

Found /fsl,dpaa/ethernet@6, Tx Channel = 62, FMAN = 1, Port ID = 1

Found /fsl,dpaa/ethernet@7, Tx Channel = 63, FMAN = 1, Port ID = 2

ERR: drivers/fman/fman.c:279:fman_if_init()

Unknown error -22: /soc@ffe000000/fman@500000/ethernet@e6000: no local-mac-address

ERR: drivers/fman/fman.c:449:fman_init()

Unknown error -22: if_init(/fsl,dpaa/ethernet@8)

Tearing down /fsl,dpaa/ethernet@5

Tearing down /fsl,dpaa/ethernet@6

Tearing down /fsl,dpaa/ethernet@7

apps/lib/usdpaa_netcfg_layer.c:488:usdpaa_netcfg_acquire(): fman driver init failed (ERRNO = -22)

error: failed to load configuration

I followed the steps given by the SDK. Any help is appreciated.

Regards,

Ankur.

Labels (1)
0 Kudos
Reply
6 Replies

1,090 Views
yipingwang
NXP TechSupport
NXP TechSupport

The application reflector is a USDPAA based sample program, please make sure that you have boot up your system with a USDPAA dtb "uImage-p4080ds-usdpaa.dtb".

Before running USDPAA application, it is required to configure frame manger for the interfaces that will receive traffic. please use FMC commands on your target before start the reflector application. for example,

$ cd /usr/etc/

$ fmc –c usdpaa_config_p4_serdes_0x10.xml –p usdpaa_policy_hash_ipv4.xml –a.

If you want to use shared MAC between USDPAA and Linux, you could use the shared MAC dtb file  p4080ds-usdpaa-shared-interfaces.dtb and shared MAC policy usdpaa_policy_hash_shared_mac_ipv4.xml.

About the Linux Kernel ping problem, please make sure fman ucode has been flashed correctly and MAC address has been configured correctly, please check whether this port can work in u-boot.

In application, please pay attention to the following configuration.

• SGMII card goes in P4080DS slot 3.

• Use SerDes 0x10 and RCW file: R_PPSXN_0x10/rcw_5g_1500mhz.bin in the

P4080DS NOR flash. This is a different RCW file than the one discussed above.

• Boot into bank 4 (assuming you are using bank 4 for USDPAA).

• Add text ";serdes:fsl_srds_lpd_b2=0xf" to u-boot environment variable hwconfig,

saveenv, and reset the system again into bank 4. This disables fm2-10g. The leading

";" separates the information added to hwconfig from what was already there. Note

that fm1-10g is never available in SerDes 0x10.

• Delete references to any of the 10 Gbps interfaces and ensure references to all

USDPAA 1 Gbps interfaces are present in the fmc configuration file. For example, it

should like the following after you edit it:

<cfgdata>

<config>

<engine name="fm1">

<port type="1G" number="0" policy="hash_ipv4_policy_5"/>

<port type="1G" number="1" policy="hash_ipv4_policy_6"/>

<port type="1G" number="2" policy="hash_ipv4_policy_7"/>

<port type="1G" number="3" policy="hash_ipv4_policy_8"/>

</engine>

</config>

</cfgdata>

Run the USDPAA application.

0 Kudos
Reply

1,090 Views
ankur
Contributor I

Thanks for your inputs, I will cross check on the dtb in use, for ping

issue some more questions

1. I am not able to ping using FM1@DTSEC2 port at all, I tried many times.

FMan was loaded, following is the boot log

2. I also do not have p4080ds-usdpaa-shared-interfaces.dtb file in image

directory, do we need to generate it by running some

special command.

U-Boot 2013.01 (Oct 21 2013 - 20:07:45)

CPU0: P4080E, Version: 3.0, (0x82080030)

Core: E500MC, Version: 3.1, (0x80230031)

Clock Configuration:

CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz,

CPU3:1499.985 MHz,

CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz,

CPU7:1499.985 MHz,

CCB:799.992 MHz,

DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999

MHz

FMAN1: 599.994 MHz

FMAN2: 599.994 MHz

QMAN: 399.996 MHz

PME: 599.994 MHz

L1: D-cache 32 kB enabled

I-cache 32 kB enabled

Reset Configuration Word (RCW):

00000000: 105a0000 00000000 1e1e181e 0000cccc

00000010: 40464000 3c3c2000 de800000 e1000000

00000020: 00000000 00000000 00000000 008b6000

00000030: 00000000 00000000 00000000 00000000

Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 4

SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz

I2C: ready

SPI: ready

DRAM: Initializing....using SPD

Detected UDIMM i-DIMM

Detected UDIMM i-DIMM

2 GiB left unmapped

4 GiB (DDR3, 64-bit, CL=9, ECC off)

DDR Controller Interleaving Mode: cache line

DDR Chip-Select Interleaving Mode: CS0+CS1

Testing 0x00000000 - 0x7fffffff

Testing 0x80000000 - 0xffffffff

Remap DDR 2 GiB left unmapped

POST memory PASSED

Flash: 128 MiB

L2: 128 KB enabled

Corenet Platform Cache: 2048 KB enabled

SERDES: bank 2 disabled

SERDES: bank 3 disabled

SRIO1: disabled

SRIO2: disabled

MMC: FSL_SDHC: 0

EEPROM: NXID v1

PCIe1: Root Complex, no link, regs @ 0xfe200000

PCIe1: Bus 00 - 00

PCIe2: disabled

PCIe3: Root Complex, x1, regs @ 0xfe202000

02:00.0 - 1095:3132 - Mass storage controller

PCIe3: Bus 01 - 02

In: serial

Out: serial

Err: serial

Net: Fman1: Uploading microcode version 106.2.9

PHY reset timed out

Fman2: Uploading microcode version 106.2.9

FM1@DTSEC2, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC3, FM2@DTSEC4

Hit any key to stop autoboot: 10 0

Thanks for your help.

Ankur.

On Fri, Nov 1, 2013 at 2:41 PM, Yiping Wang

0 Kudos
Reply

1,090 Views
yipingwang
NXP TechSupport
NXP TechSupport

Have you set these parameters in u-boot?

setenv ethact FM1@DTSEC2

setenv ethprime FM1@DTSEC2

Would you please share your u-boot environment variables and ping log?

In order to build p4080ds-usdpaa-shared-interfaces.dtb, please add "${S}/arch/powerpc/boot/dts/p4080ds-usdpaa-shared-interfaces.dts in variable  KERNEL_DEVICETREE in meta-fsl-ppc/conf/machine/p4080ds.conf.

Then rebuild Kernel.

0 Kudos
Reply

1,090 Views
ankur
Contributor I

Hi,

I have attached logs to the thread.

Regards,

Ankur.

0 Kudos
Reply

1,090 Views
yipingwang
NXP TechSupport
NXP TechSupport

I have verified your u-boot environment on my target without any problem, please check whether there is physical connection problem on your target.

0 Kudos
Reply

1,090 Views
ankur
Contributor I

Thanks for you reply.

I am attaching logs from our board.

######################################################

U-Boot 2011.12-00064-gbfb0c9a (Jun 15 2012 - 16:09:09)

CPU0: P4080E, Version: 3.0, (0x82080030)

Core: E500MC, Version: 3.1, (0x80230031)

Clock Configuration:

CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz,

CPU3:1499.985 MHz,

CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz,

CPU7:1499.985 MHz,

CCB:799.992 MHz,

DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999

MHz

FMAN1: 599.994 MHz

FMAN2: 599.994 MHz

PME: 399.996 MHz

L1: D-cache 32 kB enabled

I-cache 32 kB enabled

Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 0

36-bit Addressing

Reset Configuration Word (RCW):

00000000: 105a0000 00000000 1e1e181e 0000cccc

00000010: 40464000 3c3c2000 fe800000 61000000

00000020: 00000000 00000000 00000000 008b6000

00000030: 00000000 00000000 00000000 00000000

SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz

I2C: ready

SPI: ready

DRAM: Initializing....using SPD

Detected UDIMM i-DIMM

Detected UDIMM i-DIMM

CS2 is disabled.

CS3 is disabled.

CS2 is disabled.

CS3 is disabled.

2 GiB left unmapped

4 GiB (DDR3, 64-bit, CL=9, ECC off)

DDR Controller Interleaving Mode: cache line

DDR Chip-Select Interleaving Mode: CS0+CS1

Testing 0x00000000 - 0x7fffffff

Testing 0x80000000 - 0xffffffff

Remap DDR 2 GiB left unmapped

POST memory PASSED

Flash: 128 MiB

L2: 128 KB enabled

Corenet Platform Cache: 2048 KB enabled

SERDES: bank 2 disabled

SERDES: bank 3 disabled

SRIO1: disabled

SRIO2: disabled

MMC: FSL_SDHC: 0

EEPROM: NXID v1

PCIe1: Root Complex, no link, regs @ 0xfe200000

PCIe1: Bus 00 - 00

PCIe2: disabled

PCIe3: Root Complex, x1, regs @ 0xfe202000

02:00.0 - 1095:3132 - Mass storage controller

PCIe3: Bus 01 - 02

In: serial

Out: serial

Err: serial

Net: Fman1: Uploading microcode version 106.2.0

Fman2: Uploading microcode version 106.2.0

FM1@DTSEC2, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC3, FM2@DTSEC4

Hit any key to stop autoboot: 5 4 3 2 1 0 ÿ

U-Boot 2013.01 (Oct 21 2013 - 20:07:45)

CPU0: P4080E, Version: 3.0, (0x82080030)

Core: E500MC, Version: 3.1, (0x80230031)

Clock Configuration:

CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz,

CPU3:1499.985 MHz,

CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz,

CPU7:1499.985 MHz,

CCB:799.992 MHz,

DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999

MHz

FMAN1: 599.994 MHz

FMAN2: 599.994 MHz

QMAN: 399.996 MHz

PME: 599.994 MHz

L1: D-cache 32 kB enabled

I-cache 32 kB enabled

Reset Configuration Word (RCW):

00000000: 105a0000 00000000 1e1e181e 0000cccc

00000010: 40464000 3c3c2000 de800000 e1000000

00000020: 00000000 00000000 00000000 008b6000

00000030: 00000000 00000000 00000000 00000000

Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 4

SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz

I2C: ready

SPI: ready

DRAM: Initializing....using SPD

Detected UDIMM i-DIMM

Detected UDIMM i-DIMM

2 GiB left unmapped

4 GiB (DDR3, 64-bit, CL=9, ECC off)

DDR Controller Interleaving Mode: cache line

DDR Chip-Select Interleaving Mode: CS0+CS1

Testing 0x00000000 - 0x7fffffff

Testing 0x80000000 - 0xffffffff

Remap DDR 2 GiB left unmapped

POST memory PASSED

Flash: 128 MiB

L2: 128 KB enabled

Corenet Platform Cache: 2048 KB enabled

SERDES: bank 2 disabled

SERDES: bank 3 disabled

SRIO1: disabled

SRIO2: disabled

MMC: FSL_SDHC: 0

EEPROM: NXID v1

PCIe1: Root Complex, no link, regs @ 0xfe200000

PCIe1: Bus 00 - 00

PCIe2: disabled

PCIe3: Root Complex, x1, regs @ 0xfe202000

02:00.0 - 1095:3132 - Mass storage controller

PCIe3: Bus 01 - 02

In: serial

Out: serial

Err: serial

Net: Fman1: Uploading microcode version 106.2.9

PHY reset timed out

Fman2: Uploading microcode version 106.2.9

FM1@DTSEC2, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC3, FM2@DTSEC4

Hit any key to stop autoboot: 10 0

=> printenv

baudrate=115200

bdev=sda3

bootargs=root=/dev/nfs rw nfsroot=172.16.124.136:/home/hitachi/tftpboot/yocto

ip=172.16.124.153:172.16.124.136::255.255.255.128::eth1:off

console=ttyS0,115200 usdpaa_mem=256M,1G

bootcmd=run cboot

bootdef=bootm 0xec020000 0xed300000 0xec800000

bootdelay=10

bootfile=uImage-p4080ds.bin

c=ffe

cboot=tftp 1000000 uImage-p4080ds.bin;tftp 0x2000000

fsl-image-core-p4080ds.ext2.gz.u-boot; tftp c00000

uImage-p4080ds-usdpaa.dtb;setenv bootargs usdpaa_mem=256M

usdpaa_mem=256M,1G;bootm 1000000 0x2000000 c00000

consoledev=ttyS0

eth1addr=00:04:9F:02:85:91

eth2addr=00:04:9F:02:85:92

eth3addr=00:04:9F:02:85:93

eth4addr=00:04:9F:02:85:94

eth5addr=00:04:9F:02:85:95

eth6addr=00:04:9F:02:85:96

eth7addr=00:04:9F:02:85:97

ethact=FM1@DTSEC2

ethaddr=00:04:9F:02:85:90

ethprime=FM1@DTSEC1

fdtaddr=c00000

fdtfile=uImage-p4080ds-usdpaa.dtb

fman_ucode=0xeff40000

gateway=172.16.124.129

hwconfig=serdes:fsl_srds_lpd_b2=0xf;fsl_ddr:ctlr_intlv=cacheline,bank_intlv=cs0_cs1,ecc=off

ipaddr=172.16.124.153

loadaddr=1000000

netdev=eth1

netmask=255.255.255.128

nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath

ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off

console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp

$fdtaddr $fdtfile;bootm $loadaddr - $fdtaddr

othbootargs=bportals=s0-1 qportals=s0-1

ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate

$othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp

$fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdtaddr

ramdiskaddr=2000000

ramdiskfile=p4080ds/ramdisk.uboot

rfsaddr=0x2000000

rfsfile=fsl-image-core-p4080ds.ext2.gz.u-boot

rootpath=/home/hitachi/tftpboot/yocto

serverip=172.16.124.136

stderr=serial

stdin=serial

stdout=serial

tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize &&

erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize &&

protect on $ubootaddr +$filesize && cmp.b $loadaddr $ubootaddr $filesize

uboot=u-boot.bin

ubootaddr=0xeff80000

Environment size: 2117/8188 bytes

=> run coo boot

Using FM1@DTSEC2 device

TFTP from server 172.16.124.136; our IP address is 172.16.124.153

Filename 'uImage-p4080ds.bin'.

Load address: 0x1000000

Loading: * T T T T T T T T T T

Retry count exceeded; starting again

Using FM2@DTSEC1 device

TFTP from server 172.16.124.136; our IP address is 172.16.124.153

Filename 'uImage-p4080ds.bin'.

Load address: 0x1000000

Loading: * #################################################################

#################################################################

#################################################################

#################################################################

##########

12.9 MiB/s

done

Bytes transferred = 3956560 (3c5f50 hex)

Using FM2@DTSEC1 device

TFTP from server 172.16.124.136; our IP address is 172.16.124.153

Filename 'fsl-image-core-p4080ds.ext2.gz.u-boot'.

Load address: 0x2000000

Loading: * #################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#######################################################

13 MiB/s

done

Bytes transferred = 27522881 (1a3f741 hex)

Using FM2@DTSEC1 device

TFTP from server 172.16.124.136; our IP address is 172.16.124.153

Filename 'uImage-p4080ds-usdpaa.dtb'.

Load address: 0xc00000

Loading: * ####

10.2 MiB/s

done

Bytes transferred = 53467 (d0db hex)

WARNING: adjusting available memory to 30000000

    1. Booting kernel from Legacy Image at 01000000 ...

Image Name: Linux-3.8.13-rt9-QorIQ-SDK-V1.4

Image Type: PowerPC Linux Kernel Image (gzip compressed)

Data Size: 3956496 Bytes = 3.8 MiB

Load Address: 00000000

Entry Point: 00000000

Verifying Checksum ... OK

    1. Loading init Ramdisk from Legacy Image at 02000000 ...

Image Name: fsl-image-core-p4080ds-201310240

Image Type: PowerPC Linux RAMDisk Image (gzip compressed)

Data Size: 27522817 Bytes = 26.2 MiB

Load Address: 00000000

Entry Point: 00000000

Verifying Checksum ... OK

    1. Flattened Device Tree blob at 00c00000

Booting using the fdt blob at 0x00c00000

Uncompressing Kernel Image ... OK

Loading Ramdisk to 2e5c0000, end 2ffff701 ... OK

Loading Device Tree to 03fdf000, end 03fff0da ... OK

ERROR, usdpaa_mem arg is invalid

Using P4080 DS machine description

Memory CAM mapping: 256/256/256 Mb, residual: 3328Mb

Linux version 3.8.13-rt9-QorIQ-SDK-V1.4 (hitachi@HITTACHI-24) (gcc version

4.7.2 (GCC) ) #1 SMP Mon Oct 21 20:10:34 IST 2013

Found initrd at 0xee5c0000:0xeffff701

No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using

memblock_alloc(0000000000400000)

No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using

memblock_alloc(0000000002000000)

Qman ver:0a01,01,02

No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using

memblock_alloc(0000000001000000)

Bman ver:0a02,01,00

pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-pdsr', using

memblock_alloc(0x0000000001000000)

pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-sre', using

memblock_alloc(0x0000000000a00000)

USDPAA region at 10000000:10000000(10000:10000), 1 TLB1 entries)

CPU maps initialized for 1 thread per core

bootconsole enabled

setup_arch: bootmem

P4080 DS board from Freescale Semiconductor

arch: exit

Zone ranges:

DMA

Normal empty

HighMem

Movable zone start for each node

Early memory node ranges

node 0:

MMU: Allocated 1088 bytes of context maps for 255 contexts

PERCPU: Embedded 10 pages/cpu @c28d9000 s17216 r8192 d15552 u40960

Built 1 zonelists in Zone order, mobility grouping on. Total pages: 1040384

Kernel command line: usdpaa_mem=256M usdpaa_mem=256M,1G

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 3716020k/4194304k available (8116k kernel code, 478284k reserved,

304k data, 558k bss, 268k init)

Kernel virtual memory layout:

  • 0xfff5f000..0xfffff000 : fixmap

  • 0xffc00000..0xffe00000 : highmem PTEs

  • 0xffbfa000..0xffc00000 : early ioremap

  • 0xf1000000..0xffbfa000 : vmalloc & ioremap

Hierarchical RCU implementation.

RCU debugfs-based tracing is enabled.

NR_IRQS:512 nr_irqs:512 16

mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe040000, max 8 CPUs

mpic: ISU size: 512, shift: 9, mask: 1ff

mpic: Initializing for 512 sources

clocksource: timebase mult[14000d1b] shift[24] registered

Console: colour dummy device 80x25

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

mpic: requesting IPIs...

e500 family performance monitor hardware support registered

Brought up 8 CPUs

devtmpfs: initialized

NET: Registered protocol family 16

Found FSL PCI host bridge at 0x0000000ffe200000. Firmware bus number: 0->0

PCI host bridge /pcie@ffe200000 (primary) ranges:

MEM 0x0000000c00000000..0x0000000c1fffffff -> 0x00000000e0000000

IO 0x0000000ff8000000..0x0000000ff800ffff -> 0x0000000000000000

/pcie@ffe200000: PCICSRBAR @ 0xdf000000

/pcie@ffe200000: Setup 64-bit PCI DMA window

/pcie@ffe200000: DMA window size is 0xdf000000

EDAC PCI0: Giving out device to module 'MPC85xx_edac' controller

'mpc85xx_pci_err': DEV 'ffe200000.pcie' (INTERRUPT)

MPC85xx_edac acquired irq 482 for PCI Err

MPC85xx_edac PCI err registered

Found FSL PCI host bridge at 0x0000000ffe202000. Firmware bus number: 0->1

PCI host bridge /pcie@ffe202000 ranges:

MEM 0x0000000c40000000..0x0000000c5fffffff -> 0x00000000e0000000

IO 0x0000000ff8020000..0x0000000ff802ffff -> 0x0000000000000000

/pcie@ffe202000: PCICSRBAR @ 0xdf000000

/pcie@ffe202000: Setup 64-bit PCI DMA window

/pcie@ffe202000: DMA window size is 0xdf000000

EDAC PCI1: Giving out device to module 'MPC85xx_edac' controller

'mpc85xx_pci_err': DEV 'ffe202000.pcie' (INTERRUPT)

MPC85xx_edac acquired irq 480 for PCI Err

MPC85xx_edac PCI err registered

software IO TLB (64MB) mapped at

PCI: Probing PCI hardware

fsl-pci ffe200000.pcie: PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource

pci_bus 0000:00: root bus resource (bus

address )

pci_bus 0000:00: root bus resource

pci 0000:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)

pci 0000:00:00.0: bridge configuration invalid (), reconfiguring

pci 0000:00:00.0: PCI bridge to

fsl-pci ffe202000.pcie: PCI host bridge to bus 0001:02

pci_bus 0001:02: root bus resource (bus address

)

pci_bus 0001:02: root bus resource (bus

address )

pci_bus 0001:02: root bus resource

pci 0001:02:00.0: ignoring class 0x0b2000 (doesn't match header type 01)

PCIE error(s) detected

pci 0001:02:00.0: Primary bus is hard wired to 0

pci 0001:02:00.0: bridge configuration invalid (), reconfiguring

pci 0001:02:00.0: PCI bridge to

PCIE ERR_DR register: 0x80020000

PCIE ERR_CAP_STAT register: 0x80000001

PCIE ERR_CAP_R0 register: 0x00000800

PCIE ERR_CAP_R1 register: 0x00000000

PCIE ERR_CAP_R2 register: 0x00000000

PCIE ERR_CAP_R3 register: 0x00000000

pci 0000:00:00.0: PCI bridge to

pci 0000:00:00.0: bridge window

pci 0000:00:00.0: bridge window

pci 0001:02:00.0: BAR 9: can't assign mem pref (size 0x100000)

pci 0001:03:00.0: BAR 6: assigned

pci 0001:02:00.0: PCI bridge to

pci 0001:02:00.0: bridge window

pci 0001:02:00.0: bridge window

bio: create slab <bio-0> at 0

vgaarb: loaded

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Bman err interrupt handler present

Bman portal initialised, cpu 0

Bman portal initialised, cpu 1

Bman portal initialised, cpu 2

Bman portal initialised, cpu 3

Bman portal initialised, cpu 4

Bman portal initialised, cpu 5

Bman portal initialised, cpu 6

Bman portal initialised, cpu 7

Bman portals initialised

Bman: BPID allocator includes range 32:32

Qman err interrupt handler present

Qman portal initialised, cpu 0

Qman portal initialised, cpu 1

Qman portal initialised, cpu 2

Qman portal initialised, cpu 3

Qman portal initialised, cpu 4

Qman portal initialised, cpu 5

Qman portal initialised, cpu 6

Qman portal initialised, cpu 7

Qman portals initialised

Qman: FQID allocator includes range 256:256

Qman: FQID allocator includes range 32768:32768

Qman: CGRID allocator includes range 0:256

Qman: pool channel allocator includes range 33:15

Switching to clocksource timebase

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

rootfs image is not initramfs (no cpio magic); looks like an initrd

Freeing initrd memory: 26880k freed

fsl-rcpm ffe0e2000.global-utilities: Freescale RCPM driver

audit: initializing netlink socket (disabled)

type=2000 audit(0.492:1): initialized

bounce pool size: 64 pages

HugeTLB registered 1 MB page size, pre-allocated 0 pages

HugeTLB registered 4 MB page size, pre-allocated 0 pages

HugeTLB registered 16 MB page size, pre-allocated 0 pages

HugeTLB registered 64 MB page size, pre-allocated 0 pages

HugeTLB registered 256 MB page size, pre-allocated 0 pages

HugeTLB registered 1 GB page size, pre-allocated 0 pages

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

NTFS driver 2.1.30 .

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 654

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36) is a 16550A

console enabled, bootconsole disabled

console enabled, bootconsole disabled

serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36) is a 16550A

serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37) is a 16550A

serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37) is a 16550A

ePAPR hypervisor byte channel driver

Generic non-volatile memory driver v1.1

brd: module loaded

loop: module loaded

st: Version 20101219, fixed bufsize 32768, s/g segs 256

scsi0 : sata_sil24

scsi1 : sata_sil24

ata1: SATA max UDMA/100 host m128@0xc40000000 port 0xc40004000 irq 42

ata2: SATA max UDMA/100 host m128@0xc40000000 port 0xc40006000 irq 42

fe8000000.flash: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID

0x000001 Chip ID 0x002801

Amd/Fujitsu Extended Query Table at 0x0040

Amd/Fujitsu Extended Query version 1.3.

number of CFI chips: 1

fsl_espi ffe110000.spi: master is unqueued, this is deprecated

m25p80 spi32766.0: s25sl12801 (16384 Kbytes)

4 ofpart partitions found on MTD device spi32766.0

Creating 4 MTD partitions on "spi32766.0":

0x000000000000-0x000000100000 : "u-boot"

0x000000100000-0x000000600000 : "kernel"

0x000000600000-0x000000700000 : "dtb"

0x000000700000-0x000001000000 : "file system"

fsl_espi ffe110000.spi: at 0xf117c000 (irq = 53)

libphy: Fixed MDIO Bus: probed

platform mdio-mux-emi1.14: Driver mdio-mux-gpio requests probe deferral

platform mdio-mux-emi2.15: Driver mdio-mux-gpio requests probe deferral

libphy: Freescale PowerQUICC MII Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

FMAN(0) Fifo size settings:

- Total buffers available(512 - 256B/buffer)

- Total throughput(1Gbps)

- Max frame size(1522B)

- 1G ports TX 1(12 bufs set (min: 12))

- 1G ports RX 1(452 bufs set (min: 14))

- OH-HC ports 4(8)

- Shared extra buffers(16)

FMAN(0) open dma settings:

- Total open dma available(32)

- 1G ports TX 1(14)

- 1G ports RX 1(14)

- OH-HC ports 4(1)

- Shared extra open dma(0)

FMAN(0) Tnums settings:

- Total Tnums available(128)

- 1G ports TX 1(59)

- 1G ports RX 1(59)

- OH-HC ports 4(2)

- Shared extra tnums(2)

FMAN(1) Fifo size settings:

- Total buffers available(512 - 256B/buffer)

- Total throughput(4Gbps)

- Max frame size(1522B)

- 1G ports TX 4(12 bufs set (min: 12))

- 1G ports RX 4(104 bufs set (min: 14))

- OH-HC ports 4(8)

- Shared extra buffers(16)

FMAN(1) open dma settings:

- Total open dma available(32)

- 1G ports TX 4(4)

- 1G ports RX 4(3)

- OH-HC ports 4(1)

- Shared extra open dma(0)

FMAN(1) Tnums settings:

- Total Tnums available(128)

- 1G ports TX 4(14)

- 1G ports RX 4(15)

- OH-HC ports 4(2)

- Shared extra tnums(4)

Freescale FM module (Oct 21 2013:20:09:58), FMD API version 21.1.0

Freescale FM Ports module (Oct 21 2013:20:09:57)

dpaa_debugfs: FSL DPAA Ethernet debugfs entries ()

fsl_mac: mac.c:417:mac_load() fsl_mac: FSL FMan MAC API based driver ()

fsl_mac ffe4e0000.ethernet: FMan dTSEC version: 0x08240101

fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:04:9f:02:85:90

fsl_mac ffe4e2000.ethernet: FMan dTSEC version: 0x08240101

fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:04:9f:02:85:91

fsl_mac ffe5e0000.ethernet: FMan dTSEC version: 0x08240101

fsl_mac ffe5e0000.ethernet: FMan MAC address: 00:04:9f:02:85:95

fsl_mac ffe5e2000.ethernet: FMan dTSEC version: 0x08240101

fsl_mac ffe5e2000.ethernet: FMan MAC address: 00:04:9f:02:85:96

fsl_mac ffe5e4000.ethernet: FMan dTSEC version: 0x08240101

fsl_mac ffe5e4000.ethernet: FMan MAC address: 00:04:9f:02:85:97

fsl_mac ffe5e6000.ethernet: of_get_mac_address(/soc@ffe000000/fman@500000

/ethernet@e6000) failed

fsl_mac: probe of ffe5e6000.ethernet failed with error -22

fsl_dpa: dpaa_eth.c:4320:dpa_load() fsl_dpa: FSL DPAA Ethernet driver ()

fsl_dpa ethernet.17: Using private BM buffer pools

fsl_dpa: dpaa_eth.c:3715:dpa_rx_fq_init() Using dynamic RX QM frame queues

fsl_dpa: dpaa_eth.c:3739:dpa_tx_fq_init() Using dynamic TX QM frame queues

fsl_dpa ethernet.21: dev_get_drvdata(ffe5e6000.ethernet) failed

fsl_dpa: probe of ethernet.21 failed with error -22

fsl_oh: offline_port.c:439:oh_port_load() fsl_oh: FSL FMan Offline Parsing

port driver ()

fsl_oh dpa-fman0-oh.22: Found OH node handle compatible with fsl,dpa-oh.

fsl_oh dpa-fman0-oh.22: OH port /soc@ffe000000/fman@400000/port@82000 has

no buffer pool. Fragmentation will not be enabled

fsl_oh dpa-fman0-oh.22: OH port /soc@ffe000000/fman@400000/port@82000enabled.

e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI

e1000: Copyright (c) 1999-2006 Intel Corporation.

e1000e: Intel(R) PRO/1000 Network Driver - 2.1.4-k

e1000e: Copyright(c) 1999 - 2012 Intel Corporation.

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-pci: EHCI PCI platform driver

ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver

/soc@ffe000000/usb@210000: Invalid 'dr_mode' property, fallback to host mode

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 44, io mem 0xffe210000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

i2c /dev entries driver

mpc-i2c ffe118100.i2c: timeout 1000000 us

rtc-ds3232 0-0068: rtc core: registered ds3232 as rtc0

mpc-i2c ffe118000.i2c: timeout 1000000 us

mpc-i2c ffe119000.i2c: timeout 1000000 us

mpc-i2c ffe119100.i2c: timeout 1000000 us

EDAC MC: Ver: 3.0.0

Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software

mpc85xx_mc_err_probe: No ECC DIMMs discovered

mpc85xx_mc_err_probe: No ECC DIMMs discovered

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc0: SDHCI controller on ffe114000.sdhc using DMA

platform caam_qi.0: Linux CAAM Queue I/F driver initialised

caam ffe300000.crypto: device ID = 0x0a10030000000000 (Era -524)

caam ffe300000.crypto: job rings = 4, qi = 1

caam ffe300000.crypto: fsl,sec-v4.0 algorithms registered in /proc/crypto

platform ffe301000.jr: registering rng-caam

platform caam_qi.0: fsl,sec-v4.0 algorithms registered in /proc/crypto

Freescale USDPAA process driver

Freescale USDPAA process IRQ driver

fsl-pme ffe316000.pme: ver: 0x00100201

Freescale pme2 db driver

Freescale pme2 scan driver

fsl-pme2-scan: device pme_scan registered

Freescale hypervisor management driver

fsl-hv: no hypervisor found

IPv4 over IPv4 tunneling driver

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

NET: Registered protocol family 15

Key type dns_resolver registered

libphy: mdio_mux: probed

libphy: mdio_mux: probed

mdio-mux-gpio mdio-mux-emi1.14: Version 1.0

rtc-ds3232 0-0068: setting system clock to 2013-10-28 03:50:22 UTC

(1382932222)

ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 0)

ata1.00: ATA-8: Hitachi HDS721050CLA360, JP2OA50E, max UDMA/133

ata1.00: 976773168 sectors, multi 0: LBA48 NCQ (depth 31/32)

ata1.00: configured for UDMA/100

scsi 0:0:0:0: Direct-Access ATA Hitachi HDS72105 JP2O PQ: 0 ANSI: 5

sd 0:0:0:0: 976773168 512-byte logical blocks: (500 GB/465 GiB)

sd 0:0:0:0: Attached scsi generic sg0 type 0

sd 0:0:0:0: Write Protect is off

sd 0:0:0:0: Write cache: enabled, read cache: enabled, doesn't

support DPO or FUA

sda: unknown partition table

sd 0:0:0:0: Attached SCSI disk

ata2: SATA link down (SStatus 0 SControl 0)

RAMDISK: gzip image found at block 0

VFS: Mounted root (ext2 filesystem) readonly on device 1:0.

devtmpfs: mounted

Freeing unused kernel memory: 268k freed

INIT: version 2.88 booting

/etc/init.d/rcS: line 27: /etc/hostname: Read-only file system

Starting udev

udevd[966]: starting version 182

Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file

or directory

bootlogd.

Configuring network interfaces... done.

net.ipv4.conf.default.rp_filter = 0

net.ipv4.conf.all.rp_filter = 0

Running postinst /etc/rpm-postinsts/debianutils...

Running postinst /etc/rpm-postinsts/sysvinit-inittab...

INIT: Entering runlevel: 5

Starting Dropbear SSH server: Will output 1024 bit rsa secret key to

'/etc/dropbear/dropbear_rsa_host_key'

Generating key, this may take a while...

Public key portion is:

ssh-rsa

AAAAB3NzaC1yc2EAAAADAQABAAAAgwCi7BQQH2u2JvfBYUA10hWaN8A9b4NCIr/gkRNQewAGInOQGjgoGR96psWLrsXsOVcwFxfeDvBStM8IcevAi3lbE8v9raDfa/8ZCTWUiEmvL5ny5KU0kglqxW4lMe13k+uvjXR7cTiMfLvg7GpfA429miaByjAyDdhGZod2/jIGRp

root@p4080ds

Fingerprint: md5 dc:f5:02:08:8d:35:5e:24:2e:b3:ab:de:6a:c4:bb:b6

dropbear.

Starting network benchmark server: netserver.

Starting system log daemon...0

Starting kernel log daemon...0

Stopping Bootlog daemon: bootlogd.

Poky 9.0 (Yocto Project 1.4 Reference Distro) 1.4 p4080ds ttyS0

p4080ds login: 0xebf40000 root

root@p4080ds:~#

root@p4080ds:~#

root@p4080ds:~# cat /root/ ifcon fig

lo Link encap:Local Loopback

inet addr:127.0.0.1 Mask:255.0.0.0

inet6 addr: ::1/128 Scope:Host

UP LOOPBACK RUNNING MTU:65536 Metric:1

RX packets:0 errors:0 dropped:0 overruns:0 frame:0

TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

collisions:0 txqueuelen:0

RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

root@p4080ds:~# ifconfig -a

fm1-gb1 Link encap:Ethernet HWaddr 00:04:9f:02:85:91

BROADCAST MULTICAST MTU:1500 Metric:1

RX packets:0 errors:0 dropped:0 overruns:0 frame:0

TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

collisions:0 txqueuelen:1000

RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

Memory:fe4e2000-fe4e2fff

lo Link encap:Local Loopback

inet addr:127.0.0.1 Mask:255.0.0.0

inet6 addr: ::1/128 Scope:Host

UP LOOPBACK RUNNING MTU:65536 Metric:1

RX packets:0 errors:0 dropped:0 overruns:0 frame:0

TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

collisions:0 txqueuelen:0

RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

sit0 Link encap:UNSPEC HWaddr

00-00-00-00-00-00-10-0D-00-00-00-00-00-00-00-00

NOARP MTU:1480 Metric:1

RX packets:0 errors:0 dropped:0 overruns:0 frame:0

TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

collisions:0 txqueuelen:0

RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

tunl0 Link encap:IPIP Tunnel HWaddr

NOARP MTU:1480 Metric:1

RX packets:0 errors:0 dropped:0 overruns:0 frame:0

TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

collisions:0 txqueuelen:0

RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

######################################################

Regards,

Ankur.

On Mon, Nov 4, 2013 at 2:07 PM, Yiping Wang

0 Kudos
Reply