P4080DS ngPIXIS Actel A3P600-FGG484 fpga image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P4080DS ngPIXIS Actel A3P600-FGG484 fpga image

1,267件の閲覧回数
woyeah
Contributor I

Dear sir

Could anyone provide me  ngPIXIS A3P600-FGG484 fpga image of P4080DS board?

thanks!

best regards!

yanwang

0 件の賞賛
返信
8 返答(返信)

1,093件の閲覧回数
woyeah
Contributor I

I want to re-program the on board FPGA in P4080DS, because the board always works in hang status. 

0 件の賞賛
返信

1,093件の閲覧回数
ufedor
NXP Employee
NXP Employee

> works in hang status

What exactly does it mean?

What are states of all on-board LEDs when power is on?

0 件の賞賛
返信

1,093件の閲覧回数
woyeah
Contributor I

The P4080DS  does not switch to reset status when i press the reset button. But the power supply to board is good and LED is all on.

0 件の賞賛
返信

1,093件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide clear photo of all on-board LEDs.

0 件の賞賛
返信

1,093件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please attach separate +12V ATX connector - it is not connected in the provided picture.

0 件の賞賛
返信

1,093件の閲覧回数
woyeah
Contributor I

Attached the board with ATX power supply.P4080DS_20190531153131.jpg

0 件の賞賛
返信

1,092件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is required to use ATX2 power supply.

It must have 24-pin main connector and dedicated +12V 4-pin connector:

ATX.jpg

Both these connectors must be attached.

0 件の賞賛
返信

1,093件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please explain why the FPGA image is needed and what do you plan to do with it.

0 件の賞賛
返信