P4080DS compatibility to PSU, chassis, memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P4080DS compatibility to PSU, chassis, memory

763 次查看
mariogartner
Contributor I

I'm looking into the P4080DS (P4080 Development System) and have read it's User Guide (P4080DSUG).

Are there any recommended compatible power supply units and desktop-like chassis?

The User Guide only lists one DDR-3 memory module, and this has a "TBD" in the column "Verified?".

So which modules have actually been successfully tested?

Given that this User Guide is Revision 0 and dates back to 07/2010, is there a newer version available?

Experiences from the community about suitable PSU, chassis and memory would be useful, too.

Thank you!

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数