P4080DS compatibility to PSU, chassis, memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P4080DS compatibility to PSU, chassis, memory

753件の閲覧回数
mariogartner
Contributor I

I'm looking into the P4080DS (P4080 Development System) and have read it's User Guide (P4080DSUG).

Are there any recommended compatible power supply units and desktop-like chassis?

The User Guide only lists one DDR-3 memory module, and this has a "TBD" in the column "Verified?".

So which modules have actually been successfully tested?

Given that this User Guide is Revision 0 and dates back to 07/2010, is there a newer version available?

Experiences from the community about suitable PSU, chassis and memory would be useful, too.

Thank you!

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)