P4080 QorIQ SDK bitbake problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080 QorIQ SDK bitbake problem

Jump to solution
1,374 Views
marcmorales
Contributor I

Hello community,

I am having a problem when configuring the SDK for P4080 and setting its built image (using bitbake fsl-image-X, with X being the type of image like full, core, minimal, etc.).

Whenever I use that command i get the following repeating message:

Delaying shutdown due to active processes which appear to be holding bitbake.lock:

COMMAND  PID USER   FD   TYPE DEVICE SIZE/OFF    NODE NAME

python  2721  nxp   12u   REG    8,2        0 3435820 /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_p4080ds/bitbake.lock

python  2722  nxp   12u   REG    8,2        0 3435820 /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_p4080ds/bitbake.lock

python  2724  nxp   12u   REG    8,2        0 3435820 /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_p4080ds/bitbake.lock

python  2725  nxp   12u   REG    8,2        0 3435820 /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_p4080ds/bitbake.lock

python  2726  nxp   12u   REG    8,2        0 3435820 /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_p4080ds/bitbake.lock

python  2727  nxp   12u   REG    8,2        0 3435820 /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_p4080ds/bitbake.lock

python  2728  nxp   12u   REG    8,2        0 3435820 /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_p4080ds/bitbake.lock

python  2729  nxp   12u   REG    8,2        0 3435820 /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_p4080ds/bitbake.lock

python  2730  nxp   12u   REG    8,2        0 3435820 /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_p4080ds/bitbake.lock

Without being able to avoid this situation and after exiting the terminal, the following error appears:

WARNING: Duplicate inclusion for /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale-internal/conf/distro/imagedepends.conf in /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale-internal/conf/layer.conf

WARNING: Duplicate inclusion for /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale-internal/conf/distro/url-sha-references.conf in /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale-internal/conf/layer.conf

WARNING: Duplicate inclusion for /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-virtualization/conf/distro/include/virt_security_flags.inc in /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-virtualization/conf/layer.conf

We are stuck in this point and cannot continue with the image setting.

Any help would be kindly appreciated.

Thanks in advance,

Cheers,

Marc

Labels (1)
1 Solution
759 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Marc,

The bitbake.lock file is just used to ensure only one bitbake runs in a specific build folder at a time, as usual this file should be empty, probably your still doesn't use bitbake in a clean build environment.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
759 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Marc Morales,

If the build project wasn't created completely, the above error may occur.

Please go to the folder <install_path>/QorIQ-SDK-V1.9-20151210-yocto, remove "build_p4080ds" folder and execute the command "source ./fsl-setup-env -m p4080ds", please finish reading the EULA information and accept it, then you will enter into build_p4080ds folder automatically, please execute bitbake command.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

759 Views
marcmorales
Contributor I

Hello Yiping,

Thank you for your quick answer. I am afraid, however, that is not the solution to my problem. I now understand what happens with bitbake and successfully deleted the "build_p4080ds" folder. After proceeding to execute the commands, though, it seems that when I try to build in an image (with the bitbake command from inside the build_p4080ds folder) the bitbake.lock error persists, informing me that it is held by some processes I already specified in my original message.

I do not understand what happens with bitbake.lock, as it is created exactly after I execute the command to create the image, and the processes that seem to be holding it are inside of it?

Thank you once more and have a great day as well.

Marc

0 Kudos
760 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Marc,

The bitbake.lock file is just used to ensure only one bitbake runs in a specific build folder at a time, as usual this file should be empty, probably your still doesn't use bitbake in a clean build environment.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------