P2020 rgmii voltage ok with 3.3v?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 rgmii voltage ok with 3.3v?

1,658 Views
pauljohnson
Contributor I

It is unclear whether it is ok to operate the P2020 RGMII port at 3.3v?

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,415 Views
sureshbk
Contributor II

dear paul,

LVDD can be set to 3.3v or 2.5v which is the IO voltage of ethernet .if you change the LVDD to 3.3v , PHY also has to operate at 3.3V and all IO signals between processor and PHY should operate at 3.3V

0 Kudos
Reply

1,415 Views
pauljohnson
Contributor I

Thanks Suresh.  My concern was that the P2020EC manual states that the RGMII is spec'd for 2.5v, no mention of 3.3v.

Yes, I do have both sides at 3.3v and it is operational.

0 Kudos
Reply

1,415 Views
sureshbk
Contributor II

pastedImage_0.png

refer datasheet page 31

pastedImage_1.png

refer reference manual page 152

0 Kudos
Reply

1,415 Views
pauljohnson
Contributor I

Reference manual statement highlighted.  While it states that RGMII is defined for 2.5v, it does not state that it cannot operate at 3.3v.  I modified a board that is using GMII at 3.3v to use that same port as RGMII at 3.3v.  So far it is ok.  I suppose that the two pages that you indicated imply that since RGMII is available on the three speed Ethernet I/O it is ok to use RGMII with 3.3v.  Thanks.

pastedImage_0.png

0 Kudos
Reply