P2020 rgmii voltage ok with 3.3v?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2020 rgmii voltage ok with 3.3v?

775件の閲覧回数
pauljohnson
Contributor I

It is unclear whether it is ok to operate the P2020 RGMII port at 3.3v?

ラベル(1)
タグ(1)
0 件の賞賛
4 返答(返信)

532件の閲覧回数
sureshbk
Contributor II

dear paul,

LVDD can be set to 3.3v or 2.5v which is the IO voltage of ethernet .if you change the LVDD to 3.3v , PHY also has to operate at 3.3V and all IO signals between processor and PHY should operate at 3.3V

0 件の賞賛

532件の閲覧回数
pauljohnson
Contributor I

Thanks Suresh.  My concern was that the P2020EC manual states that the RGMII is spec'd for 2.5v, no mention of 3.3v.

Yes, I do have both sides at 3.3v and it is operational.

0 件の賞賛

532件の閲覧回数
sureshbk
Contributor II

pastedImage_0.png

refer datasheet page 31

pastedImage_1.png

refer reference manual page 152

0 件の賞賛

532件の閲覧回数
pauljohnson
Contributor I

Reference manual statement highlighted.  While it states that RGMII is defined for 2.5v, it does not state that it cannot operate at 3.3v.  I modified a board that is using GMII at 3.3v to use that same port as RGMII at 3.3v.  So far it is ok.  I suppose that the two pages that you indicated imply that since RGMII is available on the three speed Ethernet I/O it is ok to use RGMII with 3.3v.  Thanks.

pastedImage_0.png

0 件の賞賛