P1020RDB-PD: UBoot in SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1020RDB-PD: UBoot in SD card

Jump to solution
1,149 Views
abdurrehman
Contributor III

Does P1020RDB-PD support loading bootloader(uboot) from SD card?

If so, what are the switch settings to load uboot from SD card?

I am using FSL SDK 1.8. The documentation lists the procedure to burn UBoot in SD card but does not say what switch settings to use.

Thanks,
Abdur Rehman

Labels (1)
1 Solution
962 Views
addiyi
NXP Employee
NXP Employee

Please refer to Freescale Infocenter for more information.

Adrian

View solution in original post

2 Replies
963 Views
addiyi
NXP Employee
NXP Employee

Please refer to Freescale Infocenter for more information.

Adrian

617 Views
Mtvjdhfchh
Contributor I
can you offer p1020 SCH PCB BOM?
0 Kudos
Reply