Hi,
While loading one of the compiled linux kernel module on p2020 based board running on linux (fsl-image-core) uImage, I got below exception,
------------[ cut here ]------------
kernel BUG at /nobackup/chanmish/arad_for_rsp1/trunk/common/src/brcm_sdk/latest/sdk-all-6.3.4/../../../../../os/linux-qoriq-sdk/3.8-r11.1/git/arch/powerpc/include/asm/dma-mapping.h:147!
Oops: Exception in kernel mode, sig: 5 [#1]
SMP NR_CPUS=8 P2020 DS
Modules linked in: linux_kernel_bde(PO+)
NIP: f110397c LR: f1103f84 CTR: 00000000
REGS: ee631c60 TRAP: 0700 Tainted: P O (3.8.13-rt9-QorIQ-SDK-V1.5)
MSR: 00029000 <CE,EE,ME> CR: 28002222 XER: 00000000
TASK = ee5c1900[2208] 'insmod' THREAD: ee630000 CPU: 0
GPR00: f1103f84 ee631d10 ee5c1900 00800000 00000000 ef17c7f8 e00ff000 00000e00
GPR08: ff541215 00000000 00000000 ef17c7f8 88002282 10029140 c077c958 0000fff1
GPR16: c008f1c8 00000000 00000124 f1105d84 f1107d90 00000023 00000001 c07fa5bc
GPR24: ee294d40 c0840000 00000000 f110c000 ee630000 f1107ea0 f11087b8 f1107ea0
NIP [f110397c] _alloc_mpool+0x9c/0xa0 [linux_kernel_bde]
LR [f1103f84] _init+0x3b8/0x480 [linux_kernel_bde]
Call Trace:
[ee631d10] [f1107ea0] _ndevices+0x0/0xffffd098 [linux_kernel_bde] (unreliable)
[ee631d20] [f1103f84] _init+0x3b8/0x480 [linux_kernel_bde]
[ee631de0] [f110c09c] init_module+0x9c/0x178 [linux_kernel_bde]
[ee631df0] [c00021ec] do_one_initcall+0x150/0x1b8
[ee631e20] [c0091dac] load_module+0x17d8/0x1f5c
[ee631ee0] [c009261c] sys_init_module+0xec/0x14c
[ee631f40] [c000e1ac] ret_from_syscall+0x0/0x3c
--- Exception: c01 at 0xff2d0a8
LR = 0xfd2a09c
Instruction dump:
4e800020 39200000 38600000 38800000 913f08e8 48001369 907f08f0 80010014
83e1000c 38210010 7c0803a6 4e800020 <0fe00000> 9421ffe0 7c0802a6 bf810010
---[ end trace cb7b757a4229e596 ]---
Trace/breakpoint trap
root@p2020:/media/ram#
Can someone guide me how to resolve this issue? What could be going wrong here?
Regards,
-Chandra
解決済! 解決策の投稿を見る。
It is no longer allowed to use the DMA API with a NULL device.
Note that you should be contacting Broadcom for support for their code.
Where did you get the linux_kernel_bde module from?
Hi Scott,
After further investigation, I found the crash happens while calling the method "dma_alloc_coherent()". Below is the code snippet for the call in linux-kernel-bde module,
dma_addr_t dma_handle;
if (!(_dma_vbase = dma_alloc_coherent(0, alloc_size, &dma_handle, GFP_KERNEL)) || !dma_handle) {
gprintk("_alloc_mpool: Kernel failed to allocate the memory pool of size 0x%lx\n", (unsigned long)alloc_size);
return;
}
Can you provide some idea what could be the reason for failure here?
Thanks,
-Chandra
It is no longer allowed to use the DMA API with a NULL device.
Note that you should be contacting Broadcom for support for their code.
Thanks Scott. I will check with Broadcom team over this issue.
Hi Scott,
linux_kernel_bde is kernel module compiled from Broadcom SDK for their chips.
-Chandra