Is there any limitation that prevents the usage of 2 GB LAW on P1024 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any limitation that prevents the usage of 2 GB LAW on P1024 ?

Jump to solution
685 Views
radupatriu
Contributor I

Enabling a 2 GB LAW (PCI target) on a P1024rdb resets/hangs the board. I checked and there are no LAW/ATMU conflicts. Using two adjacent 1 GB LAWs for the same memory window works.

Labels (1)
0 Kudos
1 Solution
557 Views
lunminliang
NXP Employee
NXP Employee

See below technical support comment:

A 2GB LAW will behave the same way as two 1GB LAWs only when base addresses of the 2GB LAW and the first 1GB LAW are aligned to the 2GB boundary.

View solution in original post

0 Kudos
2 Replies
558 Views
lunminliang
NXP Employee
NXP Employee

See below technical support comment:

A 2GB LAW will behave the same way as two 1GB LAWs only when base addresses of the 2GB LAW and the first 1GB LAW are aligned to the 2GB boundary.

0 Kudos
557 Views
radupatriu
Contributor I

I somehow missed that.

Thanks,

Radu

0 Kudos