Basically, I want to increase elbc clock by increasing sysclk (change SW3 from sysclk= 100 MHz to 133 MHz) however I dont want to violate other system operation. To do that I need to change RCW. I dont know which part I need to change. Could you provide information for that?
Best regards.
U-Boot 2016.03 (Apr 07 2016 - 09:51:10 +0300)
CPU0: P4080E, Version: 3.0, (0x82080030)
Core: e500mc, Version: 3.1, (0x80230031)
Clock Configuration:
CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz, CPU3:1499.985 MHz,
CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz, CPU7:1499.985 MHz,
CCB:799.992 MHz,
DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999 MHz
FMAN1: 599.994 MHz
FMAN2: 599.994 MHz
QMAN: 399.996 MHz
PME: 599.994 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 105a0000 00000000 1e1e181e 0000cccc
00000010: 3842440c 3c3c2000 de800000 e1000000
00000020: 00000000 00000000 00000000 008b6000
00000030: 00000000 00000000 00000000 00000000
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 0
SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM i-DIMM
Detected UDIMM i-DIMM
2 GiB left unmapped
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
4 GiB (DDR3, 64-bit, CL=9, ECC on)
DDR Controller Interleaving Mode: cache line
DDR Chip-Select Interleaving Mode: CS0+CS1
POST memory PASSED
Flash: 128 MiB
L2: 128 KiB enabled
Corenet Platform Cache: 2 MiB enabled
SRIO1: disabled
SRIO2: disabled
MMC: FSL_SDHC: 0
EEPROM: CRC mismatch (707eb693 != ffffffff)
PCIe1: Root Complex, x1 gen1, regs @ 0xfe200000
01:00.0 - 104c:8241 - Serial bus controller
PCIe1: Bus 00 - 01
PCIe2: disabled
PCIe3: Root Complex, x1 gen1, regs @ 0xfe202000
03:00.0 - 1095:3132 - Mass storage controller
PCIe3: Bus 02 - 03
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 106.2.14
Could not get PHY for P4080DS_MDIO3: addr 4
Failed to connect
Fman2: Uploading microcode version 106.2.14
Could not get PHY for P4080DS_MDIO8: addr 30
Failed to connect
Could not get PHY for P4080DS_MDIO8: addr 31
Failed to connect
Could not get PHY for P4080DS_MDIO1: addr 0
Failed to connect
FM1@DTSEC2 [PRIME], FM1@TGEC1, FM2@DTSEC3, FM2@DTSEC4, FM2@TGEC1
Hit any key to stop autoboot: 0
=>
Please find the output of uboot above. SW3 settings default. I want to maksimum elbc (133 MHz) clock. I tihnk I need change SW3 and RCW. Could you also provide new RCW for that?
Best regards.
Please provide additional information:
1) current U-Boot output
2) desired eLBC clock frequency
Note that:
a) LCLK can't be greater than 100MHz - refer to the P4080/P4081 QorIQ Integrated Processor Hardware Specifications, Table 52. Enhanced Local Bus Timing Specifications
b) maximum LCLK frequency is equal to (Platform Clock) / 8
For the processor clocking details please refer to the P4080 QorIQ Multicore Communication Processor Reference Manual, 4.6.5 Clocking.