IF xvdd of P2041 PROCESSOR IS 1.5V DOES LA26 PIN NEED TO BE PULLED UP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IF xvdd of P2041 PROCESSOR IS 1.5V DOES LA26 PIN NEED TO BE PULLED UP?

519 Views
jagxin
Contributor III

Hai

Processor P2041

XVDD-1.5 V

In P2041 EC Free scale techinical data sheet Page no 37

29 th point The cfg_xvdd_sel (LA[26]) reset configuration pin must select the correct voltage that is being supplied on the XVDD pin

is given as note for LA26 Pin

does it mean if XVDD is used as 1.5v Pull up is needed in the line LA26 ?

Thanks and regards

AGXIN.J

Labels (1)
0 Kudos
1 Reply

304 Views
alexander_yakov
NXP Employee
NXP Employee

Yes, for XVDD = 1.5V this configuration pin should be pulled-up.

Please look P2040 Reference Manual, Section 4.6.3.5 "SerDes XVDD voltage select"

0 Kudos