I want I want to use external interrupts for P2020 in Linux. What should I do?How do I configure DTS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I want I want to use external interrupts for P2020 in Linux. What should I do?How do I configure DTS

2,187件の閲覧回数
1475849560
Contributor II

I want I want to use external interrupts for P2020 in Linux. What should I do?How do I configure DTS?

Or which documents should I look at and where to get them

dts.bmpirq.bmp

 

0 件の賞賛
返信
3 返答(返信)

2,179件の閲覧回数
bpe
NXP Employee
NXP Employee

Are you creating a totally new driver for an interrupt enabled device, or trying
to re-use an existing driver for an externally connected peripheral on P2020?

Regards,
Platon

0 件の賞賛
返信

2,177件の閲覧回数
1475849560
Contributor II

I want to create a new driver.

0 件の賞賛
返信

2,158件の閲覧回数
bpe
NXP Employee
NXP Employee

Study the recommendations given in this post. They are applicable to the processor you are working with.

 

Hope this helps,
Platon

0 件の賞賛
返信