I want I want to use external interrupts for P2020 in Linux. What should I do?How do I configure DTS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I want I want to use external interrupts for P2020 in Linux. What should I do?How do I configure DTS

2,339 次查看
1475849560
Contributor II

I want I want to use external interrupts for P2020 in Linux. What should I do?How do I configure DTS?

Or which documents should I look at and where to get them

dts.bmpirq.bmp

 

0 项奖励
回复
3 回复数

2,331 次查看
bpe
NXP Employee
NXP Employee

Are you creating a totally new driver for an interrupt enabled device, or trying
to re-use an existing driver for an externally connected peripheral on P2020?

Regards,
Platon

0 项奖励
回复

2,329 次查看
1475849560
Contributor II

I want to create a new driver.

0 项奖励
回复

2,310 次查看
bpe
NXP Employee
NXP Employee

Study the recommendations given in this post. They are applicable to the processor you are working with.

 

Hope this helps,
Platon

0 项奖励
回复