I want I want to use external interrupts for P2020 in Linux. What should I do?How do I configure DTS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want I want to use external interrupts for P2020 in Linux. What should I do?How do I configure DTS

2,234 Views
1475849560
Contributor II

I want I want to use external interrupts for P2020 in Linux. What should I do?How do I configure DTS?

Or which documents should I look at and where to get them

dts.bmpirq.bmp

 

0 Kudos
Reply
3 Replies

2,226 Views
bpe
NXP Employee
NXP Employee

Are you creating a totally new driver for an interrupt enabled device, or trying
to re-use an existing driver for an externally connected peripheral on P2020?

Regards,
Platon

0 Kudos
Reply

2,224 Views
1475849560
Contributor II

I want to create a new driver.

0 Kudos
Reply

2,205 Views
bpe
NXP Employee
NXP Employee

Study the recommendations given in this post. They are applicable to the processor you are working with.

 

Hope this helps,
Platon

0 Kudos
Reply