How to get P2020 DMA over PCIe to transmit more than one data byte per packet?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to get P2020 DMA over PCIe to transmit more than one data byte per packet?

跳至解决方案
584 次查看
toddreed
Contributor I

We have adjusted the BWC (Bandwidth/pause control bits of DMA mode register), but haven't seen any change.  We always get one data byte.  Thank you.

Todd

标签 (1)
0 项奖励
回复
1 解答
453 次查看
LPP
NXP Employee
NXP Employee

Please check the value of DMAx_MRn[DAHE,SAHE] (RM Section 13.3.1).

Probably, you are trying to DMA data to FPGA register on the PCIe side of DMA. DMA doesn't burst if DAHE,SAHE != 0.

The source/destination transaction size calculations provided in RM Section 13.4.1.1 is only applicable to the case of DAHE,SAHE = 0.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
454 次查看
LPP
NXP Employee
NXP Employee

Please check the value of DMAx_MRn[DAHE,SAHE] (RM Section 13.3.1).

Probably, you are trying to DMA data to FPGA register on the PCIe side of DMA. DMA doesn't burst if DAHE,SAHE != 0.

The source/destination transaction size calculations provided in RM Section 13.4.1.1 is only applicable to the case of DAHE,SAHE = 0.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复