How to get P2020 DMA over PCIe to transmit more than one data byte per packet?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get P2020 DMA over PCIe to transmit more than one data byte per packet?

Jump to solution
541 Views
toddreed
Contributor I

We have adjusted the BWC (Bandwidth/pause control bits of DMA mode register), but haven't seen any change.  We always get one data byte.  Thank you.

Todd

Labels (1)
0 Kudos
Reply
1 Solution
410 Views
LPP
NXP Employee
NXP Employee

Please check the value of DMAx_MRn[DAHE,SAHE] (RM Section 13.3.1).

Probably, you are trying to DMA data to FPGA register on the PCIe side of DMA. DMA doesn't burst if DAHE,SAHE != 0.

The source/destination transaction size calculations provided in RM Section 13.4.1.1 is only applicable to the case of DAHE,SAHE = 0.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
411 Views
LPP
NXP Employee
NXP Employee

Please check the value of DMAx_MRn[DAHE,SAHE] (RM Section 13.3.1).

Probably, you are trying to DMA data to FPGA register on the PCIe side of DMA. DMA doesn't burst if DAHE,SAHE != 0.

The source/destination transaction size calculations provided in RM Section 13.4.1.1 is only applicable to the case of DAHE,SAHE = 0.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply