How to do internal loopback test on UART of P1020

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to do internal loopback test on UART of P1020

1,417 次查看
sourabhdas
Contributor III

Hi, I am using P1020 RDB. I am using QorIQ-SDK-V1.7 for software development. I want to do internal loopback Test on UART during the Power-On Self Test. Our generic UART driver is not supporting internal loopback. How could I enable the internal loopback for all the UART's? If there is any reference code please share it.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,052 次查看
alexander_yakov
NXP Employee
NXP Employee

To enable internal loopback please set "LOOP" bit is the DUART_UMCRn register.

Please see P1020 Reference Manual, Section 11.3.10 for details

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复