How to disable L2-cache on P1022DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to disable L2-cache on P1022DS

965 Views
perrub
Contributor II

We are now utilizing our P1022 developent systems (P1022DS) for software component testing (unit/module testing).

We would like to extend these tests to include execution time measurements. The L2-cache is disabled in our target system, so in order to get comparable values we need to disable it for the Linux system running on the P1022DS as well. How do we proceed to achieve this?

(We use a proprietary OS for our target system, so - apparently - we lack the necessary expertise in Linux.)

Labels (1)
3 Replies

664 Views
lunminliang
NXP Employee
NXP Employee

I am afraid there is no option to do this except modify the source code.

0 Kudos
Reply

664 Views
perrub
Contributor II


I was hoping for a more convenient way, but I didn't really expect it...

From the reference manual: The L2 cache is disabled by setting L2 enable (L2E, bit 0) of the L2 Control Register (L2CTL) to 0. L2CTL is memory mapped at an offset of 0x20000 from the Configuration, Control, and Status Register Base Address.

  • How do we find out which Base Address our system use?
  • How do we actually access the L2CTL register? I suspect we need user privileges of some kind, and perhaps some kind of address processing (remapping)...?
0 Kudos
Reply

664 Views
perrub
Contributor II

We ended up writing a loadable kernel module, with the core part being these rows:

phys_addr_t L2CTL = get_immrbase() + 0x20000;

void* L2_controller = ioremap_nocache(L2CTL, 4);

iowrite8(0x50, L2_controller);

This seems to do the trick for us.