- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi All,
I am working on p1021rdb. I need to configure PB10 as gpio pin, I wrote gpios property as
gpios = <&qe_pio_b 42 0>; inside a device node.
then used following functions
of_gpio_count(),
of_get_gpio_flags(),
gpio_request(),
Here I am getting error in the of_get_gpio_flags() function call..
When I started debugging the this I came to know that QE gpio controller chip is added to the list of gpio chip controllers with only 32 gpios .
Ddue to this of_gpio_simple_xlate() is throwing error while comparing the below condition
if(gpiospec->args[0] >= gc->ngpio)
return -EINVAL;
what is the number that should be passed in the device tree to configure PB10 as gpio, is there any document that explains pin numbers and their corresponding gpio numbers in the QE gpio chip controller?
As the driver code supports only 32 gpios at max, how to port map pins? it is not like PA0 pin maps to 0, PB0 maps to 32 ??
Your help is appreciated.
Solved! Go to Solution.


- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Have a great day,
binding/powerpc/fsl/cpm_qe/gpio.txt says
#gpio-cells : Should be two. The first cell is the pin number and the second cell is used to specify optional parameters (currently unused).
as example see
lxr.free-electrons.com/source/arch/powerpc/boot/dts/mpc8569mds.dts
or
lxr.free-electrons.com/source/arch/powerpc/boot/dts/mpc8360rdk.dts
i.e. for PB10 it should be <&qe_pio_b 10 0>
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Podiatchev,
Thanks for your reply.
I understand that we need to create a node for each parallel I/O ports, and gpios property should use the proper proper port node's phandle, pin number as below..
gpios=<&qe_pio_X, pin_num, 0>
in my device tree there was only port-B node, I added port-A and tried its pins as gpios its working... :smileygrin:
Thanks once again!!


- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Have a great day,
binding/powerpc/fsl/cpm_qe/gpio.txt says
#gpio-cells : Should be two. The first cell is the pin number and the second cell is used to specify optional parameters (currently unused).
as example see
lxr.free-electrons.com/source/arch/powerpc/boot/dts/mpc8569mds.dts
or
lxr.free-electrons.com/source/arch/powerpc/boot/dts/mpc8360rdk.dts
i.e. for PB10 it should be <&qe_pio_b 10 0>
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------