How to change the NOR flash memory map in p2041rdb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change the NOR flash memory map in p2041rdb

3,186件の閲覧回数
karavindvijayak
Contributor I

We are using P2040 in our board. We are using QorIQ SDK V2.0 along with update
SDK-v2.0-1703 .

In QorIQ SDK v2.0-1703 Documentation in Table 59. NOR Flash Memory Map is Given .


How to customise this memory map if we want to use root file system with more than 44MB size

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,090件の閲覧回数
karavindvijayak
Contributor I

Is there any place in the code or compile environment where I have to make the changes for enlarging the rootfs from  0xe9300000  -  0xebefffff  to  0xe8900000 - 0xebefffff .

We have directly connected the msb ( A25 pin ) pin of flash to processor address, LA5 .  Which means we will not have alternate bank concept in our design.

In this case can we enlarge our rootfs from 0xe8900000 to 0xefefffff ..?

0 件の賞賛
返信

3,090件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello k aravind vijaya kumar,

 

If you don't use Hypervisor, you could enlarge rootfs filesystem from 0xe8900000 to 0xebefffff.

Thanks,

Yiping

0 件の賞賛
返信