How to boot P1022 u-boot into internal SRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to boot P1022 u-boot into internal SRAM

Jump to solution
3,021 Views
adriancox
Contributor III

I'm attempting to build a u-boot version for P1022 that will boot into SRAM, so that it can discover and configure any installed DIMM. I'm concerned that the standard boot file (config_ddr3_2gb_p1022ds.dat) won't work reliably on a machine fitted with a smaller or slower DIMM.

I've found and fixed the following problems, but there are more remaining. Has anybody got a configuration like this to work?

1. The config_sram_p1022ds.dat file sets the boot vector to f8f80000, rather than f8fff000 used in config_sram_p2020ds.dat

2. The u-boot config file for the P1022DS in SD boot mode sets TEXT_BASE to 0x11000000, rather than the 0xf8f80000 used in P2020DS.h

My config file:

040:424f4f54      Boot signature

044:00000000

048:00080000      Image size - should be overridden by boot-format

04c:00000000

050:00001000      Image location on SD card - should be overridden by boot-format

054:00000000

058:f8f80000      RAM address of image

05c:00000000

060:f8fff000      Start vector

064:00000000

068:00000006      Config size

080:ff720100     Set L2SRAM to f8f80000

084:f8f80000

088:ff720e44     Disable L2 cache ECC errors

08c:0000000c

090:ff720000     Enable L2 as all SRAM

094:80010000

098:ff72e40c     Set RD_SAFE on SDHC controller

09c:00000040

0a0:40000001     Delay 0x100 instruction

0a4:00000100

0a8:80000001     End configuration

0ac:80000001

My modified u-boot config section:

#ifdef CONFIG_SDCARD

#define CONFIG_RAMBOOT_SDCARD

#define CONFIG_SYS_RAMBOOT

#define CONFIG_SYS_EXTRA_ENV_RELOC

#define CONFIG_SYS_TEXT_BASE 0xf8f80000

#define CONFIG_RESET_VECTOR_ADDRESS 0xf8fffffc

#endif

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,063 Views
yipingwang
NXP TechSupport
NXP TechSupport

L2 Cache size of P1022  is 256K, but P2020's is 512K, P1022 L2 Cache for SRAM cannot accommodate the whole u-boot Image.

View solution in original post

0 Kudos
Reply
5 Replies
2,064 Views
yipingwang
NXP TechSupport
NXP TechSupport

L2 Cache size of P1022  is 256K, but P2020's is 512K, P1022 L2 Cache for SRAM cannot accommodate the whole u-boot Image.

0 Kudos
Reply
2,063 Views
adriancox
Contributor III

Thanks - I've had a go at trimming out u-boot features, but I can't get one small enough that's useful in my environment.

t looks like I'll need to get the SPL support working for SD card booting.

0 Kudos
Reply
2,063 Views
dirkeibach
Contributor II

Have a look at the controlcenterd_TRAILBLAZER board configuration. It's a trimmed u-boot configuration (not SPL) that does what you asked for.

This is our config file for booting to SRAM:

40:424f4f54

44:00000000

48:00040000

4c:00000000

50:00000400

54:00000000

58:f8fc0000

5c:00000000

60:f8fff000

64:00000000

68:00000006

80:ff720100

84:f8fc0000

88:ff720e44

8c:0000000c

90:ff720000

94:80010000

98:ff72e40c

9c:00000040

a0:40000001

a4:00000100

a8:80000001

ac:80000001

0 Kudos
Reply
2,063 Views
scottwood
NXP Employee
NXP Employee

Check out the latest upstream U-Boot (especially commit 7c8eea59b8c3b124d23b41f887bc525cf2adec30), which supports SPL for SD on P1022DS, with DDR SPD support.

0 Kudos
Reply
2,063 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to P2020DS.h to add L2 Cache configuration as the following.

    #define CONFIG_SYS_INIT_L2_ADDR>>---0xf8f80000

    #ifdef CONFIG_PHYS_64BIT

    #define CONFIG_SYS_INIT_L2_ADDR_PHYS>---0xff8f80000ull

    #else

    #define CONFIG_SYS_INIT_L2_ADDR_PHYS>---CONFIG_SYS_INIT_L2_ADDR

    #endif

    #define CONFIG_SYS_L2_SIZE>->---(512 << 10)

    #define CONFIG_SYS_INIT_L2_END>-(CONFIG_SYS_INIT_L2_ADDR + CONFIG_SYS_L2_SIZE)

    #define CONFIG_SYS_CCSRBAR>->---0xffe00000

    #define CONFIG_SYS_CCSRBAR_PHYS_LOW>CONFIG_SYS_CCSRBAR

0 Kudos
Reply