How do I update the U-Boot on P5040DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I update the U-Boot on P5040DS

750 Views
antoniogarcia
Contributor I

I have a P5040DS which currently has a u-boot built in 2013.  I need to update this to the U-boot binaries that are in the QorIQ 2.0 SDK.  I have tried to follow the instructions in section 4.4 of the QorIQ SDK Documentation.  I substitute substitute the fields such as <u-boot_start_addr> for the addresses listed in Table 18 (NOR Flash Memory Map) for the alternate u-boot bank (same for the RCW and FMAN Microcode).  However, when I do the pixis_reset altbank, the board just hangs.  Can anyone provide the exact steps to use here?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

472 Views
Pavel
NXP Employee
NXP Employee

Is recommended command sequence used from the Section 4.4.10.8 of the SDK 2.0 Documentation?

Send message dump if this command sequence is used.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

472 Views
rammurmu
Contributor III

Hi,

    Can you share the u-boot log. I have similar issue but now it is resolved.

Regards

Ram

0 Kudos
Reply