How do I change CCSBAR on P4080 CPU.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I change CCSBAR on P4080 CPU.

2,942 Views
hyenongijeong
Contributor III

This is my source code in "rominit.s" (vxWorks BSP)

Then our board is not booted.

How do I modify this code?

#define CCSBAR_RESET     0xFE000000

#define CCSBAR                    0xE0000000

/* set to ccsbar_reset in LAWBARL8 */

    WRITEADR(r6, r7, P4080_LAWBARL8(CCSBAR_RESET), CCSBAR)

    sync

    WRITEADR(r6, r7, P4080_LAWAR8(CCSBAR_RESET), (LAWAR_ENABLE | LAWAR_TGTIF_RESERVE | LAWAR_SIZE_16MB) )

    LOADVAR(r7, P4080_LAWAR8(CCSBAR_RESET))

    isync    /* ensure LAWAR8 is set */

  /* get to CCSBAR_H */

    lis     r7, HI(CCSBAR_RESET)

    ori     r7, r7, LO(CCSBAR_RESET)

    lwz     r4, (CCSRBARH_OFFSET)(r7) /* CCSRBARH_OFFSET: 0x0 */

  /* get to CCSBAR_L */

    lis     r7, HI(CCSBAR_RESET)

    ori     r7, r7, LO(CCSBAR_RESET)

    lwz     r4, (CCSRBARL_OFFSET)(r7) /* CCSRBARL_OFFSET: 0x4 */

    lis     r6, HI(CCSBAR)

    ori     r6, r6, LO(CCSBAR)

    xor     r5, r5, r5

    

    lis     r7, HI(CCSBAR_RESET)

    ori     r7, r7, LO(CCSBAR_RESET)

    stw     r5,(CCSRBARH_OFFSET)(r7) /* *(CCSBAR_RESET + CCSRBARH_OFFSET) = r5 */

    stw     r6,(CCSRBARL_OFFSET)(r7) /* *(CCSBAR_RESET + CCSRBARL_OFFSET) = r6 */

    sync

    lis     r5,HI(CCSBAR_COMMIT)

    ori     r5,r5, LO(CCSBAR_COMMIT)

    stw     r5,(CCSRAR_OFFSET)(r7)

    sync

  /* set to clear in LAWBARL8 */

    WRITEADR(r6, r7, P4080_LAWBARL8(CCSBAR), 0x0)

    sync

    WRITEADR(r6, r7, P4080_LAWAR8(CCSBAR), 0x0)

    LOADVAR(r7, P4080_LAWAR8(CCSBAR))

    isync    /* ensure LAWAR8 is set */

Labels (1)
Tags (3)
0 Kudos
Reply
4 Replies

2,366 Views
hyenongijeong
Contributor III

My Question is..

How Can I MOVE CCSBAR Address from 0xFE000000(default) to 0xE0000000 or other address?

0 Kudos
Reply

2,366 Views
ufedor
NXP Employee
NXP Employee

Please debug the code and consult with Wind River.

The NXP/Freescale solution is implemented in the U-Boot source code included into the Linux SDK:

sdk/u-boot.git - Freescale PowerPC u-boot Tree

0 Kudos
Reply

2,366 Views
hyenongijeong
Contributor III

THANK YOU FOR YOUR KIND ANSWER!

0 Kudos
Reply

2,366 Views
ufedor
NXP Employee
NXP Employee

What is the question?

0 Kudos
Reply