I've reflashed the uboot images to the latest v1.8 but i still cant seem to get the ethernet connection working. Is there a guide or something i could follow?
These are my uboot logs.
Many thanks in advance! Daniel
Hello Daniel Ng,
It looks that there is problem with RCW configuration, please configure RCW[SRDS_LPD_B2] and RCW[SRDS_LPD_B3] to disable SerDes lane 2 and 3. Actually u-boot has already provided the warningg message "Warning: SERDES8 requires banks two and three to be disabled in the RCW ".
Please use the default RCW provided in the pre-built image ISO, the attached is RCW R_PPSXX_0xe, please flash it at current bank 0xe8000000 or alternate bank 0xec000000.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------