Hi, I'm trying to resolve a Ethernet issue on the P4080ds. I've reflashed the uboot images to the latest v1.8 but i still cant see to get the ethernet connection working. Is there a guide or something i could follow? many thanks in advance! Daniel

cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I'm trying to resolve a Ethernet issue on the P4080ds. I've reflashed the uboot images to the latest v1.8 but i still cant see to get the ethernet connection working. Is there a guide or something i could follow? many thanks in advance! Daniel

1,300 Views
daniel_ng
Contributor I

I've reflashed the uboot images to the latest v1.8 but i still cant seem to get the ethernet connection working. Is there a guide or something i could follow?

These are my uboot logs.

  1. U-Boot 2015.01QorIQ-SDK-V1.8+g6ba8eed (Jun 14 2015 - 01:59:41)
  2. CPU0:  P4080E, Version: 3.0, (0x82080030)
  3. Core:  e500mc, Version: 3.1, (0x80230031)
  4. Clock Configuration:
  5.        CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz, CPU3:1499.985 M
  6.        CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz, CPU7:1499.985 M
  7.        CCB:799.992 MHz,                                                       
  8.        DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999 MHz
  9.        FMAN1: 599.994 MHz                                                     
  10.        FMAN2: 599.994 MHz                                                     
  11.        QMAN:  399.996 MHz                                                     
  12.        PME:   599.994 MHz                                                     
  13. L1:    D-cache 32 KiB enabled                                                 
  14.        I-cache 32 KiB enabled                                                 
  15. Reset Configuration Word (RCW):                                               
  16.        00000000: 105a0000 00000000 1e1e181e 0000cccc                           
  17.        00000010: 3842440c 00002000 de800000 e1000000                           
  18.        00000020: 00000000 00000000 00000000 008b6000                           
  19.        00000030: 00000000 00000000 00000000 00000000                           
  20. Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 0         
  21. SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz               
  22. I2C:   ready                                                                   
  23. SPI:   ready                                                                   
  24. DRAM:  Initializing....using SPD                                               
  25. Detected UDIMM i-DIMM                                                         
  26. Detected UDIMM i-DIMM                                                         
  27. 2 GiB left unmapped                                                           
  28. Testing 0x00000000 - 0x7fffffff                                               
  29. Testing 0x80000000 - 0xffffffff                                               
  30. Remap DDR 2 GiB left unmapped                                                 
  31.                                                                               
  32. 4 GiB (DDR3, 64-bit, CL=9, ECC on)                                             
  33.        DDR Controller Interleaving Mode: cache line                           
  34.        DDR Chip-Select Interleaving Mode: CS0+CS1                             
  35. POST memory PASSED                                                             
  36. Flash: 128 MiB                                                                 
  37. L2:    128 KiB enabled                                                         
  38. Corenet Platform Cache: 2 MiB enabled                                         
  39. Warning: SERDES8 requires banks two and three to be disabled in the RCW       
  40. SRIO1: disabled                                                               
  41. SRIO2: disabled                                                               
  42. MMC:   FSL_SDHC: 0                                                             
  43. EEPROM: CRC mismatch (ca99e036 != ffffffff)                                   
  44. PCIe1: Root Complex, no link, regs @ 0xfe200000                               
  45. PCIe1: Bus 00 - 00                                                             
  46. PCIe2: disabled                                                               
  47. PCIe3: Root Complex, x1 gen1, regs @ 0xfe202000                               
  48.   02:00.0     - 1095:3132 - Mass storage controller                           
  49. PCIe3: Bus 01 - 02                                                             
  50. In:    serial                                                                 
  51. Out:   serial                                                                 
  52. Err:   serial                                                                 
  53. Net:   Fman1: Uploading microcode version 106.2.15                             
  54. Phy 4 not found                                                               
  55. PHY reset timed out                                                           
  56. Fman2: Uploading microcode version 106.2.15                                   
  57. Phy 0 not found                                                               
  58. PHY reset timed out                                                           
  59. FM1@DTSEC2 [PRIME], FM1@TGEC1, FM2@DTSEC3, FM2@DTSEC4, FM2@TGEC1               
  60. Hit any key to stop autoboot:  0                                               
  61. WARNING: adjusting available memory to 30000000                               
  62. ## Booting kernel from Legacy Image at e8020000 ...                           
  63.    Image Name:   Linux-3.12.37-rt51-QorIQ-SDK-V1.                             
  64.    Image Type:   PowerPC Linux Kernel Image (gzip compressed)                 
  65.    Data Size:    4305061 Bytes = 4.1 MiB                                       
  66.    Load Address: 00000000                                                     
  67.    Entry Point:  00000000                                                     
  68.    Verifying Checksum ... OK                                                   
  69. ## Loading init Ramdisk from Legacy Image at e9300000 ...                     
  70.    Image Name:   fsl-image-flash-p4080ds-20150613                             
  71.    Image Type:   PowerPC Linux RAMDisk Image (gzip compressed)                 
  72.    Data Size:    8211389 Bytes = 7.8 MiB                                       
  73.    Load Address: 00000000                                                     
  74.    Entry Point:  00000000                                                     
  75.    Verifying Checksum ... OK                                                   
  76. ## Flattened Device Tree blob at e8800000                                     
  77.    Booting using the fdt blob at 0xe8800000                                   
  78.    Uncompressing Kernel Image ... OK                                           
  79.    Loading Ramdisk to 2f82b000, end 2ffffbbd ... OK                           
  80.    Loading Device Tree to 03fe3000, end 03fffdeb ... OK                       
  81. Using CoreNet Generic machine description                                     
  82. Memory CAM mapping: 256/256/256 Mb, residual: 3328Mb                           
  83. Linux version 3.12.37-rt51-QorIQ-SDK-V1.8+gf488de6 (jenkins@neptune) (gcc versi5
  84. Found initrd at 0xef82b000:0xeffffbbd                                         
  85. No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using memblock_alloc(000)
  86. No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using memblock_alloc(00)
  87. Qman ver:0a01,01,02,00                                                         
  88. No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using memblock_alloc(00)
  89. Bman ver:0a02,01,00                                                           
  90. pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-pdsr', using memblock_alloc)
  91. pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-sre', using memblock_alloc()
  92. No USDPAA memory, no 'usdpaa_mem' bootarg                                     
  93. CPU maps initialized for 1 thread per core                                     
  94. bootconsole [udbg0] enabled                                                   
  95. setup_arch: bootmem                                                           
  96. CoreNet Generic board from Freescale Semiconductor                             
  97. arch: exit                                                                     
  98. Zone ranges:                                                                   
  99.   DMA      [mem 0x00000000-0x2fffffff]                                         
  100.   Normal   empty                                                               
  101.   HighMem  [mem 0x30000000-0xffffffff]                                         
  102. Movable zone start for each node                                               
  103. Early memory node ranges                                                       
  104.   node   0: [mem 0x00000000-0xffffffff]                                       
  105. MMU: Allocated 1088 bytes of context maps for 255 contexts                     
  106. PERCPU: Embedded 8 pages/cpu @c2973000 s9664 r8192 d14912 u32768               
  107. Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 1047040   
  108. Kernel command line: root=/dev/ram rw console=ttyS0,115200                     
  109. PID hash table entries: 4096 (order: 2, 16384 bytes)                           
  110. Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)               
  111. Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)                 
  112. Sorting __ex_table...                                                         
  113. Memory: 3996472K/4194304K available (6716K kernel code, 332K rwdata, 1800K roda)
  114. Kernel virtual memory layout:                                                 
  115.   * 0xfff5f000..0xfffff000  : fixmap                                           
  116.   * 0xffc00000..0xffe00000  : highmem PTEs                                     
  117.   * 0xffbfb000..0xffc00000  : early ioremap                                   
  118.   * 0xf1000000..0xffbfb000  : vmalloc & ioremap                               
  119. Hierarchical RCU implementation.                                               
  120.         RCU debugfs-based tracing is enabled.                                 
  121. NR_IRQS:512 nr_irqs:512 16                                                     
  122. mpic: Setting up MPIC " OpenPIC  " version 1.2 at ffe040000, max 8 CPUs       
  123. mpic: ISU size: 512, shift: 9, mask: 1ff                                       
  124. mpic: Initializing for 512 sources                                             
  125. clocksource: timebase mult[14000d1b] shift[24] registered                     
  126. Console: colour dummy device 80x25                                             
  127. pid_max: default: 32768 minimum: 301                                           
  128. Mount-cache hash table entries: 512                                           
  129. mpic: requesting IPIs...                                                       
  130. e500 family performance monitor hardware support registered                   
  131. Brought up 8 CPUs                                                             
  132. devtmpfs: initialized                                                         
  133. NET: Registered protocol family 16                                             
  134.                                                                               
  135. Found FSL PCI host bridge at 0x0000000ffe200000. Firmware bus number: 0->0     
  136. PCI host bridge /pcie@ffe200000  ranges:                                       
  137. MEM 0x0000000c00000000..0x0000000c1fffffff -> 0x00000000e0000000             
  138.   IO 0x0000000ff8000000..0x0000000ff800ffff -> 0x0000000000000000             
  139. /pcie@ffe200000: PCICSRBAR @ 0xdf000000                                       
  140. /pcie@ffe200000: Setup 64-bit PCI DMA window                                   
  141. /pcie@ffe200000: DMA window size is 0xdf000000                                 
  142. EDAC PCI0: Giving out device to module 'MPC85xx_edac' controller 'mpc85xx_pci_e)
  143. MPC85xx_edac acquired irq 482 for PCI Err                                     
  144. MPC85xx_edac PCI err registered                                               
  145. Found FSL PCI host bridge at 0x0000000ffe202000. Firmware bus number: 0->1     
  146. PCI host bridge /pcie@ffe202000  ranges:                                       
  147. MEM 0x0000000c40000000..0x0000000c5fffffff -> 0x00000000e0000000             
  148.   IO 0x0000000ff8020000..0x0000000ff802ffff -> 0x0000000000000000             
  149. /pcie@ffe202000: PCICSRBAR @ 0xdf000000                                       
  150. /pcie@ffe202000: Setup 64-bit PCI DMA window                                   
  151. /pcie@ffe202000: DMA window size is 0xdf000000                                 
  152. EDAC PCI1: Giving out device to module 'MPC85xx_edac' controller 'mpc85xx_pci_e)
  153. MPC85xx_edac acquired irq 480 for PCI Err                                     
  154. MPC85xx_edac PCI err registered                                               
  155. software IO TLB [mem 0x03ff7000-0x07ff7000] (64MB) mapped at [c3ff7000-c7ff6fff]
  156. PCI: Probing PCI hardware                                                     
  157. fsl-pci ffe200000.pcie: PCI host bridge to bus 0000:00                         
  158. pci_bus 0000:00: root bus resource [io  0xf1040000-0xf104ffff] (bus address [0x)
  159. pci_bus 0000:00: root bus resource [mem 0xc00000000-0xc1fffffff] (bus address [)
  160. pci_bus 0000:00: root bus resource [bus 00-ff]                                 
  161. pci 0000:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)       
  162. pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring   
  163. pci 0000:00:00.0: PCI bridge to [bus 01-ff]                                   
  164. fsl-pci ffe202000.pcie: PCI host bridge to bus 0001:02                         
  165. pci_bus 0001:02: root bus resource [io  0xf1060000-0xf106ffff] (bus address [0x)
  166. pci_bus 0001:02: root bus resource [mem 0xc40000000-0xc5fffffff] (bus address [)
  167. pci_bus 0001:02: root bus resource [bus 02-ff]                                 
  168. pci 0001:02:00.0: ignoring class 0x0b2000 (doesn't match header type 01)       
  169. pci 0001:02:00.0: Primary bus is hard wired to 0                               
  170. pci 0001:02:00.0: bridge configuration invalid ([bus 01-01]), reconfiguring   
  171. pci 0001:02:00.0: PCI bridge to [bus 03-ff]                                   
  172. pci 0000:00:00.0: PCI bridge to [bus 01]                                       
  173. pci 0000:00:00.0:   bridge window [io  0xf1040000-0xf104ffff]                 
  174. pci 0000:00:00.0:   bridge window [mem 0xc00000000-0xc1fffffff]               
  175. pci 0001:02:00.0: BAR 9: can't assign mem pref (size 0x100000)                 
  176. pci 0001:03:00.0: BAR 6: assigned [mem 0xc40080000-0xc400fffff pref]           
  177. pci 0001:02:00.0: PCI bridge to [bus 03]                                       
  178. pci 0001:02:00.0:   bridge window [io  0xf1060000-0xf106ffff]                 
  179. pci 0001:02:00.0:   bridge window [mem 0xc40000000-0xc5fffffff]               
  180. pci_bus 0001:02: Some PCI device resources are unassigned, try booting with pcic
  181. bio: create slab <bio-0> at 0                                                 
  182. vgaarb: loaded                                                                 
  183. SCSI subsystem initialized                                                     
  184. usbcore: registered new interface driver usbfs                                 
  185. usbcore: registered new interface driver hub                                   
  186. usbcore: registered new device driver usb                                     
  187. pps_core: LinuxPPS API ver. 1 registered                                       
  188. pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@>
  189. PTP clock support registered                                                   
  190. EDAC MC: Ver: 3.0.0                                                           
  191. Bman err interrupt handler present                                             
  192. Bman portal initialised, cpu 0                                                 
  193. Bman portal initialised, cpu 1                                                 
  194. Bman portal initialised, cpu 2                                                 
  195. Bman portal initialised, cpu 3                                                 
  196. Bman portal initialised, cpu 4                                                 
  197. Bman portal initialised, cpu 5                                                 
  198. Bman portal initialised, cpu 6                                                 
  199. Bman portal initialised, cpu 7                                                 
  200. Bman portals initialised                                                       
  201. Qman err interrupt handler present                                             
  202. Qman portal initialised, cpu 0                                                 
  203. Qman portal initialised, cpu 1                                                 
  204. Qman portal initialised, cpu 2                                                 
  205. Qman portal initialised, cpu 3                                                 
  206. Qman portal initialised, cpu 4                                                 
  207. Qman portal initialised, cpu 5                                                 
  208. Qman portal initialised, cpu 6                                                 
  209. Qman portal initialised, cpu 7                                                 
  210. Qman portals initialised                                                       
  211. Bman: BPID allocator includes range 32:32                                     
  212. Qman: FQID allocator includes range 256:256                                   
  213. Qman: FQID allocator includes range 32768:32768                               
  214. Qman: CGRID allocator includes range 0:256                                     
  215. Qman: pool channel allocator includes range 33:15                             
  216. Switched to clocksource timebase                                               
  217. NET: Registered protocol family 2                                             
  218. TCP established hash table entries: 8192 (order: 4, 65536 bytes)               
  219. TCP bind hash table entries: 8192 (order: 4, 65536 bytes)                     
  220. TCP: Hash tables configured (established 8192 bind 8192)                       
  221. TCP: reno registered                                                           
  222. UDP hash table entries: 512 (order: 2, 16384 bytes)                           
  223. UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)                       
  224. NET: Registered protocol family 1                                             
  225. RPC: Registered named UNIX socket transport module.                           
  226. RPC: Registered udp transport module.                                         
  227. RPC: Registered tcp transport module.                                         
  228. RPC: Registered tcp NFSv4.1 backchannel transport module.                     
  229. Trying to unpack rootfs image as initramfs...                                 
  230. rootfs image is not initramfs (no cpio magic); looks like an initrd           
  231. Freeing initrd memory: 8016K (ef82b000 - effff000)                             
  232. audit: initializing netlink socket (disabled)                                 
  233. type=2000 audit(0.372:1): initialized                                         
  234. bounce pool size: 64 pages                                                     
  235. HugeTLB registered 1 MB page size, pre-allocated 0 pages                       
  236. HugeTLB registered 4 MB page size, pre-allocated 0 pages                       
  237. HugeTLB registered 16 MB page size, pre-allocated 0 pages                     
  238. HugeTLB registered 64 MB page size, pre-allocated 0 pages                     
  239. HugeTLB registered 256 MB page size, pre-allocated 0 pages                     
  240. HugeTLB registered 1 GB page size, pre-allocated 0 pages                       
  241. NFS: Registering the id_resolver key type                                     
  242. Key type id_resolver registered                                               
  243. Key type id_legacy registered                                                 
  244. NTFS driver 2.1.30 [Flags: R/O].                                               
  245. jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.                           
  246. msgmni has been set to 1165                                                   
  247. io scheduler noop registered                                                   
  248. io scheduler deadline registered                                               
  249. io scheduler cfq registered (default)                                         
  250. Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled                       
  251. serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36, base_baud = 24999750) is a 1A
  252. console [ttyS0] enabled, bootconsole disabled                                 
  253. console [ttyS0] enabled, bootconsole disabled                                 
  254. serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36, base_baud = 24999750) is a 1A
  255. serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37, base_baud = 24999750) is a 1A
  256. serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37, base_baud = 24999750) is a 1A
  257. ePAPR hypervisor byte channel driver                                           
  258. Generic non-volatile memory driver v1.1                                       
  259. brd: module loaded                                                             
  260. loop: module loaded                                                           
  261. st: Version 20101219, fixed bufsize 32768, s/g segs 256                       
  262. scsi0 : sata_sil24                                                             
  263. scsi1 : sata_sil24                                                             
  264. ata1: SATA max UDMA/100 host m128@0xc40000000 port 0xc40004000 irq 42         
  265. ata2: SATA max UDMA/100 host m128@0xc40000000 port 0xc40006000 irq 42         
  266. fe8000000.flash: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x01
  267. Amd/Fujitsu Extended Query Table at 0x0040                                     
  268.   Amd/Fujitsu Extended Query version 1.3.                                     
  269. number of CFI chips: 1                                                         
  270. fsl_espi ffe110000.spi: master is unqueued, this is deprecated                 
  271. m25p80 spi32766.0: s25sl12801 (16384 Kbytes)                                   
  272. 4 ofpart partitions found on MTD device spi32766.0                             
  273. Creating 4 MTD partitions on "spi32766.0":                                     
  274. 0x000000000000-0x000000100000 : "u-boot"                                       
  275. 0x000000100000-0x000000600000 : "kernel"                                       
  276. 0x000000600000-0x000000700000 : "dtb"                                         
  277. 0x000000700000-0x000001000000 : "file system"                                 
  278. fsl_espi ffe110000.spi: at 0xf117e000 (irq = 53)                               
  279. libphy: Fixed MDIO Bus: probed                                                 
  280. platform mdio-mux-emi1.14: Driver mdio-mux-gpio requests probe deferral       
  281. platform mdio-mux-emi2.15: Driver mdio-mux-gpio requests probe deferral       
  282. libphy: Freescale PowerQUICC MII Bus: probed                                   
  283. libphy: Freescale XGMAC MDIO Bus: probed                                       
  284. Freescale FM module (Jun 14 2015:02:00:31), FMD API version 21.1.0             
  285. Freescale FM Ports module (Jun 14 2015:02:00:32)                               
  286. fsl_mac: fsl_mac: FSL FMan MAC API based driver ()                             
  287. fsl_mac ffe4e0000.ethernet: FMan dTSEC version: 0x08240101                     
  288. fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:04:9f:00:67:00               
  289. fsl_mac ffe4e2000.ethernet: FMan dTSEC version: 0x08240101                     
  290. fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:04:9f:00:67:01               
  291. cpu0/0: Applying 10G TX ECC workaround (10GMAC-A004) ...                       
  292. cpu0/0: done.                                                                 
  293. fsl_mac ffe4f0000.ethernet: FMan XGEC version: 0x00010330                     
  294. fsl_mac ffe4f0000.ethernet: FMan MAC address: 00:04:9f:00:67:04               
  295. fsl_mac ffe5e4000.ethernet: FMan dTSEC version: 0x08240101                     
  296. fsl_mac ffe5e4000.ethernet: FMan MAC address: 00:04:9f:00:67:07               
  297. fsl_mac ffe5e6000.ethernet: FMan dTSEC version: 0x08240101                     
  298. fsl_mac ffe5e6000.ethernet: FMan MAC address: 00:04:9f:00:67:08               
  299. cpu0/0: Applying 10G TX ECC workaround (10GMAC-A004) ...                       
  300. cpu0/0: done.                                                                 
  301. fsl_mac ffe5f0000.ethernet: FMan XGEC version: 0x00010330                     
  302. fsl_mac ffe5f0000.ethernet: FMan MAC address: 00:04:9f:00:67:09               
  303. fsl_dpa: FSL DPAA Ethernet driver ()                                           
  304. fsl_dpa: FSL DPAA Ethernet debugfs entries ()                                 
  305. fsl_dpa: fsl_dpa: Probed interface eth0                                       
  306. fsl_dpa: fsl_dpa: Probed interface eth1                                       
  307. fsl_dpa: fsl_dpa: Probed interface eth2                                       
  308. fsl_dpa: fsl_dpa: Probed interface eth3                                       
  309. fsl_dpa: fsl_dpa: Probed interface eth4                                       
  310. fsl_advanced: FSL DPAA Advanced drivers: ()                                   
  311. fsl_proxy: FSL DPAA Proxy initialization driver ()                             
  312. fsl_dpa_shared: FSL DPAA Shared Ethernet driver ()                             
  313. fsl_dpa_macless: FSL DPAA MACless Ethernet driver ()                           
  314. fsl_oh: FSL FMan Offline Parsing port driver ()                               
  315. e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI               
  316. e1000: Copyright (c) 1999-2006 Intel Corporation.                             
  317. e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k                             
  318. e1000e: Copyright(c) 1999 - 2013 Intel Corporation.                           
  319. ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver                     
  320. ehci-pci: EHCI PCI platform driver                                             
  321. ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver                         
  322. ohci-pci: OHCI PCI platform driver                                             
  323. /soc@ffe000000/usb@210000: Invalid 'dr_mode' property, fallback to host mode   
  324. fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller                   
  325. fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1             
  326. fsl-ehci fsl-ehci.0: irq 44, io mem 0xffe210000                               
  327. fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00                               
  328. hub 1-0:1.0: USB hub found                                                     
  329. hub 1-0:1.0: 1 port detected                                                   
  330. usbcore: registered new interface driver usb-storage                           
  331. i2c /dev entries driver                                                       
  332. mpc-i2c ffe118100.i2c: timeout 1000000 us                                     
  333. rtc-ds3232 0-0068: rtc core: registered ds3232 as rtc0                         
  334. mpc-i2c ffe118000.i2c: timeout 1000000 us                                     
  335. mpc-i2c ffe119000.i2c: timeout 1000000 us                                     
  336. mpc-i2c ffe119100.i2c: timeout 1000000 us                                     
  337. Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software                 
  338. EDAC MC0: Giving out device to 'MPC85xx_edac' 'mpc85xx_mc_err': DEV mpc85xx_mc_r
  339. MPC85xx_edac acquired irq 490 for MC                                           
  340. MPC85xx_edac MC err registered                                                 
  341. EDAC MC1: Giving out device to 'MPC85xx_edac' 'mpc85xx_mc_err': DEV mpc85xx_mc_r
  342. MPC85xx_edac acquired irq 489 for MC                                           
  343. MPC85xx_edac MC err registered                                                 
  344. sdhci: Secure Digital Host Controller Interface driver                         
  345. sdhci: Copyright(c) Pierre Ossman                                             
  346. sdhci-pltfm: SDHCI platform and OF driver helper                               
  347. mmc0: SDHCI controller on ffe114000.sdhc [ffe114000.sdhc] using DMA           
  348. platform caam_qi.0: Linux CAAM Queue I/F driver initialised                   
  349. caam ffe300000.crypto: device ID = 0x0a10030000000000 (Era 4)                 
  350. caam ffe300000.crypto: job rings = 4, qi = 1                                   
  351. caam algorithms registered in /proc/crypto                                     
  352. platform caam_qi.0: fsl,sec-v4.0 algorithms registered in /proc/crypto         
  353. caam_jr ffe301000.jr: registering rng-caam                                     
  354. caam ffe300000.crypto: fsl,sec-v4.0 algorithms registered in /proc/crypto     
  355. Freescale USDPAA process driver                                               
  356. fsl-usdpaa: no region found                                                   
  357. Freescale USDPAA process IRQ driver                                           
  358. fsl-pme ffe316000.pme: ver: 0x00100201                                         
  359. Freescale pme2 db driver                                                       
  360. Freescale pme2 scan driver                                                     
  361. fsl-pme2-scan: device pme_scan registered                                     
  362. Freescale hypervisor management driver                                         
  363. fsl-hv: no hypervisor found                                                   
  364. ipip: IPv4 over IPv4 tunneling driver                                         
  365. TCP: cubic registered                                                         
  366. Initializing XFRM netlink socket                                               
  367. NET: Registered protocol family 10                                             
  368. sit: IPv6 over IPv4 tunneling driver                                           
  369. NET: Registered protocol family 17                                             
  370. NET: Registered protocol family 15                                             
  371. 8021q: 802.1Q VLAN Support v1.8                                               
  372. Key type dns_resolver registered                                               
  373. libphy: mdio_mux: probed                                                       
  374. libphy: mdio_mux: probed                                                       
  375. mdio-mux-gpio mdio-mux-emi1.14: Version 1.0                                   
  376. libphy: mdio_mux: probed                                                       
  377. mdio_bus ffe4f1000: MDIO read error                                           
  378. mdio_bus ffe4f1000: MDIO read error                                           
  379. mdio_bus ffe4f1000: MDIO read error                                           
  380. mdio_bus ffe4f1000: MDIO read error                                           
  381. mdio_bus 1.1: cannot get PHY at address 0                                     
  382. libphy: mdio_mux: probed                                                       
  383. mdio_bus ffe4f1000: MDIO read error                                           
  384. mdio_bus ffe4f1000: MDIO read error                                           
  385. mdio_bus ffe4f1000: MDIO read error                                           
  386. mdio_bus ffe4f1000: MDIO read error                                           
  387. mdio_bus 1.3: cannot get PHY at address 4                                     
  388. mdio-mux-gpio mdio-mux-emi2.15: Version 1.0                                   
  389. fsl_generic: FSL DPAA Generic Ethernet driver ()                               
  390. fsl_generic: FSL DPAA Ethernet debugfs entries ()                             
  391. rtc-ds3232 0-0068: setting system clock to 2015-08-05 10:40:43 UTC (1438771243)
  392. ata1: SATA link down (SStatus 0 SControl 0)                                   
  393. ata2: SATA link down (SStatus 0 SControl 0)                                   
  394. RAMDISK: gzip image found at block 0                                           
  395. VFS: Mounted root (ext2 filesystem) on device 1:0.                             
  396. devtmpfs: mounted                                                             
  397. Freeing unused kernel memory: 276K (c0855000 - c089a000)                       
  398. INIT: version 2.88 booting                                                     
  399. Starting udev                                                                 
  400. udevd[1118]: starting version 182                                             
  401. Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or y
  402. bootlogd.                                                                     
  403. Populating dev cache                                                           
  404. Running postinst /etc/rpm-postinsts/100-util-linux-readprofile...             
  405. Running postinst /etc/rpm-postinsts/101-sysvinit-inittab...                   
  406. update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing)   
  407. INIT: Entering runlevel: 5                                                     
  408. Configuring network interfaces... done.                                       
  409. Starting OpenBSD Secure Shell server: sshd
  410. root@p4080ds:~# ifconfig
  411. lo        Link encap:Local Loopback 
  412.           inet addr:127.0.0.1  Mask:255.0.0.0
  413.           inet6 addr: ::1/128 Scope:Host
  414.           UP LOOPBACK RUNNING  MTU:65536  Metric:1
  415.           RX packets:0 errors:0 dropped:0 overruns:0 frame:0
  416.           TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
  417.           collisions:0 txqueuelen:0
  418.           RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
  419. => printenv                                                                   
  420. baudrate=115200                                                               
  421. bdev=sda1                                                                     
  422. bootcmd=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othboot0
  423. bootdelay=3                                                                   
  424. bootfile=uImage                                                               
  425. consoledev=ttyS0                                                               
  426. eth1addr=00:04:9f:00:67:01                                                     
  427. eth2addr=00:04:9f:00:67:02                                                     
  428. eth3addr=00:04:9f:00:67:03                                                     
  429. eth4addr=00:04:9f:00:67:04                                                     
  430. eth5addr=00:04:9f:00:67:05                                                     
  431. eth6addr=00:04:9f:00:67:06                                                     
  432. eth7addr=00:04:9f:00:67:07                                                     
  433. eth8addr=00:04:9f:00:67:08                                                     
  434. eth9addr=00:04:9f:00:67:09                                                     
  435. ethact=FM1@DTSEC2                                                             
  436. ethaddr=00:04:9f:00:67:00                                                     
  437. ethprime=FM1@DTSEC2                                                           
  438. fdtaddr=c00000                                                                 
  439. fdtfile=uImage-p4080ds.dtb                                                     
  440. fman_ucode=eff00000                                                           
  441. gatewayip=192.168.1.1                                                         
  442. hvboot=setenv bootargs console=ttyS0,115200 config-addr=0xfe8900000;bootm 0xfe80
  443. hwconfig=fsl_ddr:ctlr_intlv=cacheline,bank_intlv=cs0_cs1;fsl_fm1_xaui_ph,addr_he
  444. ipaddr=192.168.1.101                                                           
  445. loadaddr=1000000                                                               
  446. netdev=eth0                                                                   
  447. netmask=255.255.255.0                                                         
  448. nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddrr
  449. ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootr
  450. ramdiskaddr=2000000                                                           
  451. ramdiskfile=fsl-image-flash-p4080ds.ext2.gz.u-boot                             
  452. rootpath=/opt/nfsroot                                                         
  453. sataboot=setenv bootargs root=/dev/sda1 rootdelay=5 rw console=$consoledev,$bau0
  454. serverip=192.168.1.100                                                         
  455. stderr=serial                                                                 
  456. stdin=serial                                                                   
  457. stdout=serial                                                                 
  458. tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erae
  459. uboot=u-boot-P4080DS.bin                                                       
  460. ubootaddr=0xeff80000                                                           
  461.                                                                               
  462. Environment size: 1919/8188 bytes

Many thanks in advance! Daniel

Labels (1)
Tags (2)
0 Kudos
1 Reply

212 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Daniel Ng,

It looks that there is problem with RCW configuration, please configure RCW[SRDS_LPD_B2] and RCW[SRDS_LPD_B3] to disable SerDes lane 2 and 3. Actually u-boot has already provided the warningg message  "Warning: SERDES8 requires banks two and three to be disabled in the RCW ".

Please use the default RCW provided in the pre-built image ISO, the attached is RCW R_PPSXX_0xe, please flash it at current bank 0xe8000000 or alternate bank 0xec000000.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos