#################################################################################################################################
Freescale Linux-Oriented Software Development Kit
#################################################################################################################################
[install the SDK]
How to install Yocto on the host machine.
1. Mount the ISO on your machine:
$ sudo mount -o loop QorIQ-SDK-V1.3-<target>-<yyyymmdd>-yocto.iso /mnt/cdrom
2. As a non-root user, install the Yocto:
$ /mnt/cdrom/install
3. When you are prompted to input the install path, ensure that the current user has the correct permission for the install path.
[Host Environment]
How to Set up the Host Environment for doing a build with Yocto.
The following steps are used to prepare the environment for doing a build with Yocto:
1.
$ cd <yocto_install_path>
2.
$ . /scripts/host-prepare.sh
3.
$ source ./fsl-setup-poky -m <machine> -j [# of bitbake jobs] -t [# of makethreads]
For example:
* $ source ./fsl-setup-poky -m p4080ds -j 12 -t 12 -l
[Builds]
How to Set up a Cross Build Environment and Perform Builds
Follow these steps to do builds using Yocto. Be sure to set up the host environment before doing these steps.
1.
$ cd <yocto_install_path>/build_<machine>_release/
2.
$ bitbake <image-target>
Where <image-target> is one of the following:
* fsl-image-minimal: contains basic packages to boot up a board
* fsl-image-core: contains common open source packages and Freescale-specific packages.
* fsl-image-full: contains all packages in the full package list.
* fsl-image-flash: contains all the user space apps needed to deploy the fsl-image-full image to a USB stick, hard drive, or other large physical media.
* fsl-image-kvm: contains guest rootfs in qemu
* fsl-toolchain: the cross compiler binary package
* package-name(usdpaa): build a specific package
#################################################################################################################################
Before the last step(#bitbake fsl-image-minimal),everthing goes well.Below is my log.
#################################################################################################################################
[mgkiller@localhost QorIQ-SDK-V1.3-20121114-yocto]$
[mgkiller@localhost QorIQ-SDK-V1.3-20121114-yocto]$
[mgkiller@localhost QorIQ-SDK-V1.3-20121114-yocto]$ source ./fsl-setup-poky -m p4080ds -j 12 -t 12 -l
Configuring for p4080ds board type
Run the following commands to start a build:
bitbake fsl-image-lsb-sdk
bitbake fsl-image-minimal
bitbake fsl-image-core
bitbake fsl-image-flash
bitbake fsl-image-kvm
bitbake fsl-image-full
To return to this build environment later please run:
source /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/SOURCE_THIS
[mgkiller@localhost build_p4080ds_release]$
[mgkiller@localhost build_p4080ds_release]$
[mgkiller@localhost build_p4080ds_release]$ bitbake fsl-image-minimal
Pseudo is not present but is required, building this first before the main build
DEBUG: Removed the following variables from the environment: SSH_ASKPASS, GNOME_DESKTOP_SESSION_ID, LESSOPEN, QT_IM_MODULE, INPUTRC, SHLVL, G_BROKEN_FILENAMES, HISTSIZE, WINDOWID, XMODIFIERS, BBFETCH2, USERNAME, GDM_XSERVER_LOCATION, GDMSESSION, GTK_IM_MODULE, BUILDDIR, HOSTNAME, CVS_RSH, MAIL, LS_COLORS
DEBUG: Found bblayers.conf (/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/conf/bblayers.conf)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/conf/bblayers.conf
DEBUG: Adding layer /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/layer.conf
DEBUG: Adding layer /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-yocto
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-yocto/conf/layer.conf
DEBUG: Adding layer /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/layer.conf
DEBUG: Adding layer /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc-private
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc-private/conf/layer.conf
DEBUG: Adding layer /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-oe/meta-oe
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-oe/meta-oe/conf/layer.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/bitbake.conf
DEBUG: CONF conf/bitbake.conf:652: including conf/abi_version.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/abi_version.conf
DEBUG: CONF conf/bitbake.conf:653: including conf/site.conf
DEBUG: CONF file 'conf/site.conf' not found
DEBUG: CONF conf/bitbake.conf:654: including conf/auto.conf
DEBUG: CONF file 'conf/auto.conf' not found
DEBUG: CONF conf/bitbake.conf:655: including conf/local.conf
DEBUG: LOAD conf/local.conf
DEBUG: CONF conf/bitbake.conf:656: including conf/build/i686-linux.conf
DEBUG: CONF file 'conf/build/i686-linux.conf' not found
DEBUG: CONF conf/bitbake.conf:657: including conf/target/INVALID-oe-linux.conf
DEBUG: CONF file 'conf/target/INVALID-oe-linux.conf' not found
DEBUG: CONF conf/bitbake.conf:658: including conf/machine/p4080ds.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/machine/p4080ds.conf
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/machine/p4080ds.conf:4: including e500mc.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/machine/e500mc.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/machine/e500mc.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/machine/e500mc.inc:3: including conf/machine/include/tune-ppce500mc.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/machine/include/tune-ppce500mc.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/machine/include/tune-ppce500mc.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/machine/include/tune-ppce500mc.inc:3: including conf/machine/include/powerpc/arch-powerpc.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/machine/include/powerpc/arch-powerpc.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/machine/include/powerpc/arch-powerpc.inc
DEBUG: CONF conf/bitbake.conf:659: including conf/machine-sdk/${SDKMACHINE}.conf
DEBUG: CONF file 'conf/machine-sdk/${SDKMACHINE}.conf' not found
DEBUG: CONF conf/bitbake.conf:660: including conf/distro/fsl.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/distro/fsl.conf
DEBUG: CONF conf/bitbake.conf:661: including conf/distro/defaultsetup.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:1: including conf/distro/include/default-providers.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-providers.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-providers.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:2: including conf/distro/include/default-versions.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-versions.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-versions.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:3: including conf/distro/include/default-distrovars.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-distrovars.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-distrovars.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:4: including conf/distro/include/world-broken.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/world-broken.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/world-broken.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:7: including conf/distro/include/tcmode-default.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/tcmode-default.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/tcmode-default.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/tcmode-default.inc:59: including conf/distro/include/as-needed.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/as-needed.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/as-needed.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:10: including conf/distro/include/tclibc-eglibc.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/tclibc-eglibc.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/tclibc-eglibc.inc
DEBUG: CONF conf/bitbake.conf:662: including conf/documentation.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/documentation.conf
DEBUG: CONF conf/bitbake.conf:663: including conf/sanity.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/sanity.conf
DEBUG: BB configuration INHERITs:0: inheriting classes/base.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:3: inheriting classes/patch.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/patch.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/patch.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/patch.bbclass:8: inheriting classes/terminal.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/terminal.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/terminal.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:4: inheriting classes/staging.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/staging.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/staging.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:6: inheriting classes/mirrors.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/mirrors.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/mirrors.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:7: inheriting classes/utils.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/utils.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/utils.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:8: inheriting classes/utility-tasks.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/utility-tasks.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/utility-tasks.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:9: inheriting classes/metadata_scm.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/metadata_scm.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/metadata_scm.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:10: inheriting classes/logging.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/logging.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/logging.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/rm_work.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/rm_work.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/rm_work.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/own-mirrors.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/own-mirrors.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/own-mirrors.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/package_rpm.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package_rpm.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package_rpm.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package_rpm.bbclass:1: inheriting classes/package.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package.bbclass:41: inheriting classes/packagedata.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/packagedata.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/packagedata.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package.bbclass:42: inheriting classes/prserv.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/prserv.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/prserv.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/buildstats.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/buildstats.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/buildstats.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/image-mklibs.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/image-mklibs.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/image-mklibs.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/image-prelink.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/image-prelink.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/image-prelink.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/insane.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/insane.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/insane.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/debian.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/debian.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/debian.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/devshell.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/devshell.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/devshell.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/sstate.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/sstate.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/sstate.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/license.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/license.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/license.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/sanity.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/sanity.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/sanity.bbclass
DEBUG: Clearing SRCREV cache due to cache policy of: clear
DEBUG: Using cache in '/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/cache/bb_codeparser.dat' for codeparser cache
WARNING: Host distribution "CentOS release 5.4 (Final)" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
DEBUG: Fetcher accessed the network with the command git ls-remote git://git.yoctoproject.org/yocto-firewall-test HEAD
DEBUG: Running export HOME="/home/mgkiller"; export SSH_AGENT_PID="3552"; export SSH_AUTH_SOCK="/tmp/ssh-oerzmI3517/agent.3517"; export GIT_CONFIG="/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux/etc/gitconfig"; export PATH="/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux/usr/bin/ppce500mc-fsl-linux:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/p4080ds/usr/bin/crossscripts:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux/usr/sbin:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux/usr/bin:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux/sbin:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux//bin:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/bitbake/bin/:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/scripts:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/bitbake/bin/:/usr/kerberos/bin:/usr/local/bin:/usr/bin:/bin:/usr/X11R6/bin:/home/mgkiller/bin:/usr/crosstool/usr/bin:/usr/local/bin:/sbin:/usr/bin/yum:/home/mgkiller/QorIQ_SDK-20110709-systembuilder/freescale-2010.09/bin/:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/scripts"; git ls-remote git://git.yoctoproject.org/yocto-firewall-test HEAD
ERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:
Failed to fetch test data from the network. Please ensure your network is configured correctly.
ERROR: Execution of event handler 'check_sanity_eventhandler' failed
DEBUG: Removed the following variables from the environment: SSH_ASKPASS, GNOME_DESKTOP_SESSION_ID, LESSOPEN, QT_IM_MODULE, INPUTRC, SHLVL, G_BROKEN_FILENAMES, HISTSIZE, WINDOWID, XMODIFIERS, BBFETCH2, USERNAME, GDM_XSERVER_LOCATION, GDMSESSION, GTK_IM_MODULE, BUILDDIR, HOSTNAME, CVS_RSH, MAIL, LS_COLORS
DEBUG: Found bblayers.conf (/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/conf/bblayers.conf)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/conf/bblayers.conf
DEBUG: Adding layer /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/layer.conf
DEBUG: Adding layer /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-yocto
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-yocto/conf/layer.conf
DEBUG: Adding layer /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/layer.conf
DEBUG: Adding layer /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc-private
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc-private/conf/layer.conf
DEBUG: Adding layer /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-oe/meta-oe
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-oe/meta-oe/conf/layer.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/bitbake.conf
DEBUG: CONF conf/bitbake.conf:652: including conf/abi_version.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/abi_version.conf
DEBUG: CONF conf/bitbake.conf:653: including conf/site.conf
DEBUG: CONF file 'conf/site.conf' not found
DEBUG: CONF conf/bitbake.conf:654: including conf/auto.conf
DEBUG: CONF file 'conf/auto.conf' not found
DEBUG: CONF conf/bitbake.conf:655: including conf/local.conf
DEBUG: LOAD conf/local.conf
DEBUG: CONF conf/bitbake.conf:656: including conf/build/i686-linux.conf
DEBUG: CONF file 'conf/build/i686-linux.conf' not found
DEBUG: CONF conf/bitbake.conf:657: including conf/target/INVALID-oe-linux.conf
DEBUG: CONF file 'conf/target/INVALID-oe-linux.conf' not found
DEBUG: CONF conf/bitbake.conf:658: including conf/machine/p4080ds.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/machine/p4080ds.conf
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/machine/p4080ds.conf:4: including e500mc.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/machine/e500mc.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/machine/e500mc.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/machine/e500mc.inc:3: including conf/machine/include/tune-ppce500mc.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/machine/include/tune-ppce500mc.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/machine/include/tune-ppce500mc.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/machine/include/tune-ppce500mc.inc:3: including conf/machine/include/powerpc/arch-powerpc.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/machine/include/powerpc/arch-powerpc.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/machine/include/powerpc/arch-powerpc.inc
DEBUG: CONF conf/bitbake.conf:659: including conf/machine-sdk/${SDKMACHINE}.conf
DEBUG: CONF file 'conf/machine-sdk/${SDKMACHINE}.conf' not found
DEBUG: CONF conf/bitbake.conf:660: including conf/distro/fsl.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta-fsl-ppc/conf/distro/fsl.conf
DEBUG: CONF conf/bitbake.conf:661: including conf/distro/defaultsetup.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:1: including conf/distro/include/default-providers.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-providers.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-providers.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:2: including conf/distro/include/default-versions.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-versions.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-versions.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:3: including conf/distro/include/default-distrovars.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-distrovars.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/default-distrovars.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:4: including conf/distro/include/world-broken.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/world-broken.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/world-broken.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:7: including conf/distro/include/tcmode-default.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/tcmode-default.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/tcmode-default.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/tcmode-default.inc:59: including conf/distro/include/as-needed.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/as-needed.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/as-needed.inc
DEBUG: CONF /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/defaultsetup.conf:10: including conf/distro/include/tclibc-eglibc.inc
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/tclibc-eglibc.inc: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/distro/include/tclibc-eglibc.inc
DEBUG: CONF conf/bitbake.conf:662: including conf/documentation.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/documentation.conf
DEBUG: CONF conf/bitbake.conf:663: including conf/sanity.conf
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/conf/sanity.conf
DEBUG: BB configuration INHERITs:0: inheriting classes/base.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:3: inheriting classes/patch.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/patch.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/patch.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/patch.bbclass:8: inheriting classes/terminal.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/terminal.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/terminal.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:4: inheriting classes/staging.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/staging.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/staging.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:6: inheriting classes/mirrors.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/mirrors.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/mirrors.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:7: inheriting classes/utils.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/utils.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/utils.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:8: inheriting classes/utility-tasks.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/utility-tasks.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/utility-tasks.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:9: inheriting classes/metadata_scm.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/metadata_scm.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/metadata_scm.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/base.bbclass:10: inheriting classes/logging.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/logging.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/logging.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/rm_work.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/rm_work.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/rm_work.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/own-mirrors.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/own-mirrors.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/own-mirrors.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/package_rpm.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package_rpm.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package_rpm.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package_rpm.bbclass:1: inheriting classes/package.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package.bbclass:41: inheriting classes/packagedata.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/packagedata.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/packagedata.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/package.bbclass:42: inheriting classes/prserv.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/prserv.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/prserv.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/buildstats.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/buildstats.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/buildstats.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/image-mklibs.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/image-mklibs.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/image-mklibs.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/image-prelink.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/image-prelink.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/image-prelink.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/insane.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/insane.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/insane.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/debian.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/debian.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/debian.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/devshell.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/devshell.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/devshell.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/sstate.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/sstate.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/sstate.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/license.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/license.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/license.bbclass
DEBUG: BB configuration INHERITs:0: inheriting classes/sanity.bbclass
DEBUG: BB /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/sanity.bbclass: handle(data, include)
DEBUG: LOAD /home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/meta/classes/sanity.bbclass
DEBUG: Clearing SRCREV cache due to cache policy of: clear
DEBUG: Using cache in '/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/cache/bb_codeparser.dat' for codeparser cache
WARNING: Host distribution "CentOS release 5.4 (Final)" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
DEBUG: Fetcher accessed the network with the command git ls-remote git://git.yoctoproject.org/yocto-firewall-test HEAD
DEBUG: Running export HOME="/home/mgkiller"; export SSH_AGENT_PID="3552"; export SSH_AUTH_SOCK="/tmp/ssh-oerzmI3517/agent.3517"; export GIT_CONFIG="/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux/etc/gitconfig"; export PATH="/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux/usr/bin/ppce500mc-fsl-linux:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/p4080ds/usr/bin/crossscripts:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux/usr/sbin:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux/usr/bin:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux/sbin:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/build_p4080ds_release/tmp/sysroots/i686-linux//bin:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/bitbake/bin/:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/scripts:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/bitbake/bin/:/usr/kerberos/bin:/usr/local/bin:/usr/bin:/bin:/usr/X11R6/bin:/home/mgkiller/bin:/usr/crosstool/usr/bin:/usr/local/bin:/sbin:/usr/bin/yum:/home/mgkiller/QorIQ_SDK-20110709-systembuilder/freescale-2010.09/bin/:/home/mgkiller/QorIQ-SDK-V1.3-20121114-yocto/scripts"; git ls-remote git://git.yoctoproject.org/yocto-firewall-test HEAD
ERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:
Failed to fetch test data from the network. Please ensure your network is configured correctly.
ERROR: Execution of event handler 'check_sanity_eventhandler' failed
[mgkiller@localhost build_p4080ds_release]$
#################################################################################################################################
What is the problem?
I need some help,anyone tell me?
Is it necessary for me to connet my PC to Internet?
My PC for work is forbidened to connect to Internet ,what shound I do?
#################################################################################################################################