Flashing uboot onto P1024 without JTAG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flashing uboot onto P1024 without JTAG

跳至解决方案
728 次查看
pavankumarg
Contributor II

Hi,

I am currently using a P1024RDB .The board currently uses boot image from NOR flash. Does the P1024RDB support flashing of u-boot onto the board without a JTAG (serial or other methods if any). I want to flash my own u-boot image on the board for testing the peripherals.

Thanks.

标签 (1)
标记 (4)
0 项奖励
1 解答
568 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

U-boot itself can program NOR flash. U-boot may download image into memory, erase flash and write image to the flash. Please see

https://www.denx.de/wiki/view/DULG/UBootInstallUsingUBoot Check u-boot commands

The P1024RDB NOR flash can be split into two logical halves by setting the FBANK_SEL signal. The FBANK_SEL signal is controlled by setting SW4[8]. It also has NAND flash. So you can write your u-boot image without erasing the original.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
569 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

U-boot itself can program NOR flash. U-boot may download image into memory, erase flash and write image to the flash. Please see

https://www.denx.de/wiki/view/DULG/UBootInstallUsingUBoot Check u-boot commands

The P1024RDB NOR flash can be split into two logical halves by setting the FBANK_SEL signal. The FBANK_SEL signal is controlled by setting SW4[8]. It also has NAND flash. So you can write your u-boot image without erasing the original.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励