Enable NTPD in p2041rdb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable NTPD in p2041rdb

1,782 Views
avinashh
Contributor III

Hi ,

I want to enable ntpd in p2041rdb. How to enable ntpd in p2041rdb. I am using kernel which came in yocto sdk v1.9. any option is there in kernel configuration or any patch is available for that ?

Labels (1)
2 Replies

1,586 Views
Pavel
NXP Employee
NXP Employee

Look at attached snapshot about NTP supporting. It is snapshot of kernel menu from this SDK.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,586 Views
avinashh
Contributor III

Hi Pavel,

Thanks for your reply.

Actually I have enabled that option in menucofing. But when system booted, it shows " <path to hctosys.c>: unable to open rtc device(rtc0)" and "</dev/misc/rtc no such file or directory.". I am using Micro Crystal's RV-3029 rtc chip connected to i2c 0 bus. I have also enabled Micro Crystal driver in the menuconfig and disabled Dallas rtc driver. but the error is same. 

0 Kudos
Reply