Difference b/w P2020RDB_NAND and P2020RDB-PC_NAND?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference b/w P2020RDB_NAND and P2020RDB-PC_NAND?

947件の閲覧回数
fahadarslan
Contributor II

Hi,

What is the difference between P2020RDB_NAND and P2020RDB-PC_NAND. Can the image containing PC be run on P2020RDB target?

Version info for the board I'm using is as below

From U-Boot:

CPU0:  P2020E, Version: 2.0, (0x80ea0020)

Core:  E500, Version: 5.0, (0x80211050)

And from sticker at bottom side of board:

P2020RDB-PB REV B

Thanks,

Fahad

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

789件の閲覧回数
scottwood
NXP Employee
NXP Employee

They target different board revisions.  If you have a -PB board then you need to use the P2020RDB_NAND target.

0 件の賞賛
返信

789件の閲覧回数
fahadarslan
Contributor II

SDK 1.3.2 for QorIQ processors supports P2020RDB-PC board, is P2020RDB-PB obsolete? And what exactly is the difference between -PB and -PC boards, is it related to hardware or can firmware updates be used to upgrade to -PC?

Thanks,

Fahad

0 件の賞賛
返信

789件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

There are hardware differences between PB and PC, PC fixes some erratas of PB and improved in layout.

For example, the PB board supports DDR2 and the PC board has been designed to support DDR3.

0 件の賞賛
返信