How do I get a single DDR3 Chip (Alliance Memory AS4C128M16D3) running on a P1014? Are there any examples?
Have a great day,
AS4C128M16D3 is a 16-bit DDR3 JEDEC Standard Compliant device which is supported by the P1014. I am not sure what do you mean as "get a single DDR3 Chip (Alliance Memory AS4C128M16D3) running on a P1014”. Do you mean connections, layout example or register settings problem? Unfortunately I did not see the right example. But I believe the next application notes can be useful
AN3940, Hardware and Layout Design Considerations for DDR3 SDRAM Memory Interfaces
https://www.freescale.com/webapp/Download?colCode=AN3940
AN4039, PowerQUICC and QorIQ DDR3 SDRAM Controller Register Setting Considerations
http://cache.freescale.com/files/32bit/doc/app_note/AN4039.pdf
See also section 4 DDR controller recommendations in the AN4534, P1010 QorIQ Integrated Processor Design Checklist
https://www.freescale.com/webapp/Download?colCode=AN4534
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for your reply. AN4039 helped a lot.