Could not load the image on P4080DS Hypervisor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Could not load the image on P4080DS Hypervisor

5,769 次查看
peterzheng
Contributor II

Hi,

I was trying to create 8 partition by editing the hv.dts file. But currently after boot up into Hypervisor, it shows the error of "Could not load the image". As shown below,

[0] =======================================                                    
[0] Freescale Hypervisor 1.3-009                                               
[0] Hypervisor command line: config-addr=0xfe8900000 console=ttyS0,115200      
[0] malloc_init: using 14100 KiB at 0x7f130150 - 0x7fef4fff                    
[0] malloc_init: using 1060 KiB at 0x7fef6000 - 0x7fffefff                     
[0] dt_read_aliases: Alias pci1 points to non-existent /pcie@ffe201000         
[0] read_pma: phys-mem-area lnx1_pma is not a power of two                     
[6] read_pma: phys-mem-area lnx7_pma is not a power of two                     
[3] read_pma: phys-mem-area lnx4_pma is not a power of two                     
[7] read_pma: phys-mem-area lnx8_pma is not a power of two                     
[1] read_pma: phys-mem-area lnx2_pma is not a power of two                     
[2] read_pma: phys-mem-area lnx3_pma is not a power of two                     
[0] read_pma: phys-mem-area lnx1_pma is not a power of two                     
[5] read_pma: phys-mem-area lnx6_pma is not a power of two                     
[4] read_pma: phys-mem-area lnx5_pma is not a power of two                     
[0] assign_callback: device buffer-pool@7 in buffer-pool@7 not found           
[0] assign_callback: device buffer-pool@8 in buffer-pool@8 not found           
[0] assign_callback: device buffer-pool@9 in buffer-pool@9 not found           
[0] assign_callback: device buffer-pool@16 in buffer-pool@16 not found         
[0] assign_callback: device buffer-pool@17 in buffer-pool@17 not found         
[0] assign_callback: device /fsl,dpaa/ethernet@16 in dpa-ethernet@16 not found 
[0] assign_callback: device /fsl,dpaa/dpa-fman0-oh@1 in dpa-fman0-oh@1 not found
[1] get_rpn: mem-range has unmapped guest address at 0x0.                      
[1] get_rpn: mem-range has unmapped guest address at 0x0.                      
[1] get_rpn: mem-range has unmapped guest address at 0x0.                      
[1] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] hv_pamu_config_liodn: liodn 146 or device in use                           
[0] configure_liodn: config of liodn failed (rc=-259)                          
[0] hv_pamu_config_liodn: liodn 146 or device in use                           
[0] configure_liodn: config of liodn failed (rc=-259)                          
[0] hv_pamu_config_liodn: liodn 146 or device in use                           
[0] configure_liodn: config of liodn failed (rc=-259)                          
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] get_rpn: mem-range has unmapped guest address at 0x0.                      
[0] Loading uImage from 0xfe9300000 to 0x1300000                               
[2] Loading uImage from 0xfe9300000 to 0x1300000                               
[3] Loading uImage from 0xfe9300000 to 0x1300000                               
[1] Loading uImage from 0xfe9300000 to 0x1300000                               
[2] copy_phys_to_gphys: cannot map dest 1300000, 0 bytes                       
[5] Loading uImage from 0xfe9300000 to 0x1300000                               
[2] load_uimage: cannot copy                                                   
[1] copy_phys_to_gphys: cannot map dest 1300000, 0 bytes                       
[3] copy_phys_to_gphys: cannot map dest 1300000, 0 bytes                       
[5] copy_phys_to_gphys: cannot map dest 1300000, 0 bytes                       
[6] Loading uImage from 0xfe9300000 to 0x1300000                               
[1] load_uimage: cannot copy                                                   
[3] load_uimage: cannot copy                                                   
[4] Loading uImage from 0xfe9300000 to 0x1300000                               
[6] copy_phys_to_gphys: cannot map dest 1300000, 0 bytes                       
[0] copy_phys_to_gphys: cannot map dest 1300000, 0 bytes                       
[3] guest p4-linux: could not load image                                       
[5] load_uimage: cannot copy                                                   
[7] Loading uImage from 0xfe9300000 to 0x1300000                               
[1] guest p2-linux: could not load image                                       
[2] guest p3-linux: could not load image                                       
[4] copy_phys_to_gphys: cannot map dest 1300000, 0 bytes                       
[6] load_uimage: cannot copy                                                   
[0] load_uimage: cannot copy                                                   
[3] loading binary image from 0xfe8020000 to 0                                 
[5] guest p6-linux: could not load image                                       
[6] guest p7-linux: could not load image                                       
[1] loading binary image from 0xfe8020000 to 0                                 
[7] copy_phys_to_gphys: cannot map dest 1300000, 0 bytes                       
[0] guest p1-linux: could not load image                                       
[3] copy_phys_to_gphys: cannot map dest 0, 0 bytes                             
[2] loading binary image from 0xfe8020000 to 0                                 
[1] copy_phys_to_gphys: cannot map dest 0, 0 bytes                             
[3] guest p4-linux: could not load image                                       
[6] loading binary image from 0xfe8020000 to 0                                 
[7] load_uimage: cannot copy                                                   
[4] load_uimage: cannot copy                                                   
[7] guest p8-linux: could not load image                                       
[1] guest p2-linux: could not load image                                       
[2] copy_phys_to_gphys: cannot map dest 0, 0 bytes                             
[4] guest p5-linux: could not load image                                       
[5] loading binary image from 0xfe8020000 to 0                                 
[6] copy_phys_to_gphys: cannot map dest 0, 0 bytes                             
[0] loading binary image from 0xfe8020000 to 0                                 
[2] guest p3-linux: could not load image                                       
[5] copy_phys_to_gphys: cannot map dest 0, 0 bytes                             
[0] copy_phys_to_gphys: cannot map dest 0, 0 bytes                             
[5] guest p6-linux: could not load image                                       
[4] loading binary image from 0xfe8020000 to 0                                 
[6] guest p7-linux: could not load image                                       
[4] copy_phys_to_gphys: cannot map dest 0, 0 bytes                             
[7] loading binary image from 0xfe8020000 to 0                                 
[0] guest p1-linux: could not load image                                       
[7] copy_phys_to_gphys: cannot map dest 0, 0 bytes                             
[4] guest p5-linux: could not load image                                       
[7] guest p8-linux: could not load image                                       
HV>                                                                            


I was following this document Section 4.2.1.6. Hypervisor Deployment

http://cache.freescale.com/files/soft_dev_tools/doc/support_info/QorIQ-SDK-1.6-IC-RevB.pdf


Here are the command I used, are they correct?


.2.1.6 Hypervisor Deployment


4.2.1.6.1 Introduction


At the U-Boot prompt, set the environment:

=>setenv bootargs config-addr=0xfe8900000 console=ttyS0,115200

=>setenv bootcmd 'bootm 0xfe8700000 - 0xfe8800000'

=>saveenv


4.2.1.6.2

switch to bank 4(assume alt bank)

1. Program kernel to flashtftp 1000000 /tftpboot/p4080ds/u-boot-P4080DS-2014.01+fslgit-r0.bin


=>tftp 1000000 /tftpboot/p4080ds/uImage

=>erase e8020000 +$filesize

=>cp.b 1000000 e8020000 $filesize


2. Program ramdisk filesystem to Flash


=>tftp 1000000 /tftpboot/p4080ds/fsl-image-core-p4080ds.tar.gz

=>erase e9300000 +$filesize

=>cp.b 1000000 e9300000 $filesize


3. Program Hypervisor image to Flash

=>tftp 1000000 /tftpboot/p4080ds/hv/hv.uImage

=>erase e8700000 +$filesize

=>cp.b 1000000 e8700000 $filesize


4. Program Kernel dtb to flash

=>tftp 1000000 /tftpboot/yocto/boot/p4080ds-usdpaa.dtb

=>erase e8800000 +$filesize

=>cp.b 1000000 e8800000 $filesize


5. Program HV dtb to Flash

=>tftp 1000000 /tftpboot/p4080ds/hv-cfg/R_PPSXX_0xe/hv-2p-lnx-lnx.dtb

=>erase e8900000 +$filesize

=>cp.b 1000000 e8900000 $filesize


6. Booting up DS board

=>boot

Is there anything I did wrong? Did I transfer the wrong file?

Thanks,

Peter

标签 (1)
标记 (2)
0 项奖励
回复
16 回复数

5,336 次查看
scottwood
NXP Employee
NXP Employee

That log shows a lot of errors in the hv config tree that need to be fixed.

0 项奖励
回复

5,336 次查看
peterzheng
Contributor II

Can u help me take a look at my hv.dts file? Thanks

0 项奖励
回复

5,336 次查看
scottwood
NXP Employee
NXP Employee

Please attach your hv.dts if you'd like me to look at it.

0 项奖励
回复

5,336 次查看
peterzheng
Contributor II

Hi Scott,

Thank you for your help. Attached is my dts file. I was trying to create 8 partitions.


Regards,

Peter

0 项奖励
回复

5,336 次查看
scottwood
NXP Employee
NXP Employee

As the error messages say, you have PMAs that are not powers of two.  This is not allowed (largely due to the relationship between PMAs and coherency subdomains).  If you want a partition to have a non-power-of-two memory size you need to use multiple PMAs.  A lot of the other error messages are consequences of having invalid PMAs.

0 项奖励
回复

5,336 次查看
peterzheng
Contributor II

Hi Scott,

I have modified the size of PMA into 128MB, but it seems the problem remains. Can you help me take a look?

Here are the error message at boot-up:

[0] =======================================                               
[0] Freescale Hypervisor 1.3-009                                          
[0] Hypervisor command line: config-addr=0xfe8900000 console=ttyS0,115200 
[0] malloc_init: using 14096 KiB at 0x7f131150 - 0x7fef4fff               
[0] malloc_init: using 1060 KiB at 0x7fef6000 - 0x7fffefff                
[0] dt_read_aliases: Alias pci1 points to non-existent /pcie@ffe201000    
[0] read_pma: phys-mem-area lnx2_pma is not naturally aligned             
[2] read_pma: phys-mem-area lnx3_pma is not naturally aligned             
[1] read_pma: phys-mem-area lnx2_pma is not naturally aligned             
[0] assign_callback: device buffer-pool@16 in buffer-pool@16 not found    
[0] assign_callback: device buffer-pool@17 in buffer-pool@17 not found    

[0] assign_callback: device /fsl,dpaa/ethernet@16 in dpa-ethernet@16 not found 

[1] get_rpn: mem-range has unmapped guest address at 0x0.                 
[1] get_rpn: mem-range has unmapped guest address at 0x0.                 
[1] get_rpn: mem-range has unmapped guest address at 0x0.                 
[1] get_rpn: mem-range has unmapped guest address at 0x0.                 
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] hv_pamu_config_liodn: liodn 146 or device in use                      
[0] configure_liodn: config of liodn failed (rc=-259)                     
[0] hv_pamu_config_liodn: liodn 146 or device in use                      
[0] configure_liodn: config of liodn failed (rc=-259)                     
[0] hv_pamu_config_liodn: liodn 146 or device in use                      
[0] configure_liodn: config of liodn failed (rc=-259)                     
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.           
[0] Loading uImage from 0xfe9300000 to 0x1300000                          
[3] Loading uImage from 0xfe9300000 to 0x1300000                          
[2] Loading uImage from 0xfe9300000 to 0x1300000                          
[6] Loading uImage from 0xfe9300000 to 0x1300000                          
[2] copy_phys_to_gphys: cannot map dest 1300000, 0 bytes                  
[4] Loading uImage from 0xfe9300000 to 0x1300000                          
[7] Loading uImage from 0xfe9300000 to 0x1300000                          
[1] Loading uImage from 0xfe9300000 to 0x1300000                          
[2] load_uimage: cannot copy                                              
[5] Loading uImage from 0xfe9300000 to 0x1300000                          
[1] copy_phys_to_gphys: cannot map dest 1300000, 0 bytes                  
[2] guest p3-linux: could not load image                                  
[1] load_uimage: cannot copy                                              
[1] guest p2-linux: could not load image                                  
[2] Loading uImage from 0xfe8020000 to 0                                  
[2] load_uimage: image size exceeds target window                         
[1] Loading uImage from 0xfe8020000 to 0                                  
[2] guest p3-linux: could not load image                                  
[1] load_uimage: image size exceeds target window                         
[1] guest p2-linux: could not load image                                  
HV> info                                                                  
Partition   Name    State     Vcpus                               
-------------------------------------------                               
1       p1-linuxstarting     1                                
2       p2-linuxstopped     1                                 
3       p3-linuxstopped     1                                 
4       p4-linuxstarting     1                                
5       p5-linuxstarting     1                                
6       p6-linuxstarting     1                                
7       p7-linuxstarting     1                                
8       p8-linuxstarting     1                                
HV> info                                                                  
Partition   Name    State     Vcpus                               
-------------------------------------------                               
1       p1-linuxstarting     1                                
2       p2-linuxstopped     1                                 
3       p3-linuxstopped     1                                 
4       p4-linuxstarting     1                                
5       p5-linuxstarting     1                                
6       p6-linuxstarting     1                                
7       p7-linuxstarting     1                                
8       p8-linuxstarting     1                                
[6] Loading uImage from 0xfe8020000 to 0                                  
[6] load_uimage: image size exceeds target window                         
[3] Loading uImage from 0xfe8020000 to 0                                  
[6] guest p7-linux: could not load image                                  
[3] load_uimage: image size exceeds target window                         
[3] guest p4-linux: could not load image                                  
[7] Loading uImage from 0xfe8020000 to 0                                  
[7] load_uimage: image size exceeds target window                         
[4] Loading uImage from 0xfe8020000 to 0                                  
[4] load_uimage: image size exceeds target window                         
[7] guest p8-linux: could not load image                                  
[4] guest p5-linux: could not load image                                  
[5] Loading uImage from 0xfe8020000 to 0                                  
[5] load_uimage: image size exceeds target window                         
[5] guest p6-linux: could not load image                                  
[0] Loading uImage from 0xfe8020000 to 0                                  
[0] load_uimage: image size exceeds target window                         
[0] guest p1-linux: could not load image                                  
HV> info                                                                  
Partition   Name    State     Vcpus                               
-------------------------------------------                               
1       p1-linuxstopped     1                                 
2       p2-linuxstopped     1                                 
3       p3-linuxstopped     1                                 
4       p4-linuxstopped     1                                 
5       p5-linuxstopped     1                                 
6       p6-linuxstopped     1                                 
7       p7-linuxstopped     1                                 
8       p8-linuxstopped     1                                 

HV>

And attached is my updated hv.dts.

Thanks & Regards,

Peter

0 项奖励
回复

5,336 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Peter,

It seems there is problem with lnx2_pma size definition in hv.dts file.

Please refer to the following hypervisor code for the error " phys-mem-area lnx2_pma is not naturally aligned"

        if (pma->start & (pma->size - 1)) {

printlog(LOGTYPE_PARTITION, LOGLEVEL_ERROR,

"%s: phys-mem-area %s is not naturally aligned\n",

__func__, node->name);

                goto out_free;

        }

Thanks,

Yiping

0 项奖励
回复

5,336 次查看
peterzheng
Contributor II

Hi Yiping,

Thank you for your reply. Could you suggest how can I modify the corresponding pma to pass this error?

Also, for the other error, could you help take a look as well?

Thank you very much for your help.

Regards,

Peter

0 项奖励
回复

5,336 次查看
scottwood
NXP Employee
NXP Employee

Natural alignment means the pma needs to be aligned to its size.  If your PMA is 128 MiB, it needs to be aligned to an 128 MiB boundary.  The other errors may be a consequence of this one, so address this one first.

0 项奖励
回复

5,336 次查看
peterzheng
Contributor II

Hi Scott,

I have fixed the alignment issue. But still cannot boot up.Would you mind taking a look again?

[0] =======================================
[0] Freescale Hypervisor 1.3-009
[0] Hypervisor command line: config-addr=0xfe8900000 console=ttyS0,115200
[0] malloc_init: using 14096 KiB at 0x7f131150 - 0x7fef4fff
[0] malloc_init: using 1060 KiB at 0x7fef6000 - 0x7fffefff
[0] dt_read_aliases: Alias pci1 points to non-existent /pcie@ffe201000
[0] assign_callback: device buffer-pool@16 in buffer-pool@16 not found
[0] assign_callback: device buffer-pool@17 in buffer-pool@17 not found
[0] assign_callback: device /fsl,dpaa/ethernet@16 in dpa-ethernet@16 not found
[1] get_rpn: mem-range has unmapped guest address at 0x8000000.
[1] get_rpn: mem-range has unmapped guest address at 0x8000000.
[1] get_rpn: mem-range has unmapped guest address at 0x8000000.
[1] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] hv_pamu_config_liodn: liodn 146 or device in use
[0] configure_liodn: config of liodn failed (rc=-259)
[0] hv_pamu_config_liodn: liodn 146 or device in use
[0] configure_liodn: config of liodn failed (rc=-259)
[0] hv_pamu_config_liodn: liodn 146 or device in use
[0] configure_liodn: config of liodn failed (rc=-259)
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] get_rpn: mem-range has unmapped guest address at 0x8000000.
[0] Loading uImage from 0xfe9300000 to 0x1300000
[1] Loading uImage from 0xfe9300000 to 0x1300000
[3] Loading uImage from 0xfe9300000 to 0x1300000
[6] Loading uImage from 0xfe9300000 to 0x1300000
[7] Loading uImage from 0xfe9300000 to 0x1300000
[2] Loading uImage from 0xfe9300000 to 0x1300000
[4] Loading uImage from 0xfe9300000 to 0x1300000
[5] Loading uImage from 0xfe9300000 to 0x1300000
HV> info
Partition   Name        State         Vcpus
-------------------------------------------
1           p1-linux    starting         1
2           p2-linux    starting         1
3           p3-linux    starting         1
4           p4-linux    starting         1
5           p5-linux    starting         1
6           p6-linux    starting         1
7           p7-linux    starting         1
8           p8-linux    starting         1
HV> info
Partition   Name        State         Vcpus
-------------------------------------------
1           p1-linux    starting         1
2           p2-linux    starting         1
3           p3-linux    starting         1
4           p4-linux    starting         1
5           p5-linux    starting         1
6           p6-linux    starting         1
7           p7-linux    starting         1
8           p8-linux    starting         1
[1] Loading uImage from 0xfe8020000 to 0
[1] load_uimage: image size exceeds target window
[1] guest p2-linux: could not load image
[3] Loading uImage from 0xfe8020000 to 0
[3] load_uimage: image size exceeds target window
[3] guest p4-linux: could not load image
[7] Loading uImage from 0xfe8020000 to 0
[7] load_uimage: image size exceeds target window
[7] guest p8-linux: could not load image
[6] Loading uImage from 0xfe8020000 to 0
[6] load_uimage: image size exceeds target window
[6] guest p7-linux: could not load image
[2] Loading uImage from 0xfe8020000 to 0
[2] load_uimage: image size exceeds target window
[2] guest p3-linux: could not load image
[4] Loading uImage from 0xfe8020000 to 0
[4] load_uimage: image size exceeds target window
[4] guest p5-linux: could not load image
[5] Loading uImage from 0xfe8020000 to 0
[5] load_uimage: image size exceeds target window
[5] guest p6-linux: could not load image
[0] Loading uImage from 0xfe8020000 to 0
[0] load_uimage: image size exceeds target window
[0] guest p1-linux: could not load image
HV>


Btw, attached is the uImage I used, It was flashed using the following command before.

=>tftp 1000000 /tftpboot/p4080ds/uImage--3.12-r0-p4080ds-20150311135235.bin

=>erase e8020000 +$filesize

=>cp.b 1000000 e8020000 $filesize

Could this because the uImage was wrong? Then which file in the build folder should I flash?

Thanks,

Peter

!

0 项奖励
回复

5,336 次查看
scottwood
NXP Employee
NXP Employee

Please attach your updated hv.dts.

0 项奖励
回复

5,336 次查看
peterzheng
Contributor II

Hi Scott,

Attached is the updated hv.dts file.

Regards,

Peter

0 项奖励
回复

5,336 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Peter,

In the dts file, you need to modify the lnx2_pma allocation as the following.

lnx2_pma: lnx2_pma {
compatible = "phys-mem-area";
addr = <0x0 0x08000000>;    // Linux
size = <0x0 0x08000000>;    // 128MB
//PETER:allocate cpc-way to it
allocate-cpc-ways = <4 5 6 7>;

    };

The address 0xe8020000 is the current bank address, you need to jump to the altbank and do flash programming here.

Would you please also provide your u-boot log(including u-boot setup log, your actions performing and hypervisor setup log) to let us do more investigation?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

5,327 次查看
peterzheng
Contributor II

Hi Yiping,

Thank you for your reply. I have made the change you suggest on the alignment issue. But it seems the problem remains.

As required, following the the u-boot log:

U-Boot 2014.01QorIQ-SDK-V1.6+gfe1d4f5 (Jun 08 2014 - 23:29:25)                 
                                                                               
CPU0:  P4080E, Version: 3.0, (0x82080030)                                     
Core:  e500mc, Version: 3.1, (0x80230031)                                     
Clock Configuration:                                                           
      CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz, CPU3:1499.985 MH
z,                                                                             
      CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz, CPU7:1499.985 MH
z,                                                                             
      CCB:799.992 MHz,                                                       
      DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999 MHz
      FMAN1: 599.994 MHz                                                     
      FMAN2: 599.994 MHz                                                     
      QMAN:  399.996 MHz                                                     
      PME:  599.994 MHz                                                     
L1:    D-cache 32 KiB enabled                                                 
      I-cache 32 KiB enabled                                                 
Reset Configuration Word (RCW):                                               
      00000000: 105a0000 00000000 1e1e181e 0000cccc                           
      00000010: 3842440c 3c3c2000 de800000 e1000000                           
      00000020: 00000000 00000000 00000000 008b6000                           
      00000030: 00000000 00000000 00000000 00000000                           
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 0         
SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz               
I2C:  ready                                                                   
SPI:  ready                                                                   
DRAM:  Initializing....using SPD                                               
Detected UDIMM i-DIMM                                                         
Detected UDIMM i-DIMM                                                         
2 GiB left unmapped                                                           
4 GiB (DDR3, 64-bit, CL=9, ECC on)                                             
      DDR Controller Interleaving Mode: cache line                           
      DDR Chip-Select Interleaving Mode: CS0+CS1                             
Testing 0x00000000 - 0x7fffffff                                               
Testing 0x80000000 - 0xffffffff                                               
Remap DDR 2 GiB left unmapped                                                 
                                                                               
POST memory PASSED                                                             
Flash: 128 MiB                                                                 
L2:    128 KiB enabled                                                         
Corenet Platform Cache: 2 MiB enabled                                         
SRIO1: disabled                                                               
SRIO2: disabled                                                               
MMC:  FSL_SDHC: 0                                                             
EEPROM: NXID v1                                                               
PCIe1: Root Complex, no link, regs @ 0xfe200000                               
PCIe1: Bus 00 - 00                                                             
PCIe2: disabled                                                               
PCIe3: Root Complex, x1 gen1, regs @ 0xfe202000                               
  02:00.0    - 1095:3132 - Mass storage controller                           
PCIe3: Bus 01 - 02                                                             
In:    serial                                                                 
Out:  serial                                                                 
Err:  serial                                                                 
Net:  Fman1: Uploading microcode version 106.2.14                             
Phy not found                                                                 
PHY reset timed out                                                           
Fman2: Uploading microcode version 106.2.14                                   
Phy not found                                                                 
PHY reset timed out                                                           
FM1@DTSEC2 [PRIME], FM1@TGEC1, FM2@DTSEC3, FM2@DTSEC4, FM2@TGEC1               
Hit any key to stop autoboot:  0                                               
=>        

And this is the boot up environment:

=> pri                                                                         
baudrate=115200                                                               
bdev=sda1                                                                     
bootargs=config-addr=0xfe8900000 console=ttyS0,115200                         
bootcmd=bootm 0xfe8700000 - 0xfe8800000                                       
bootdelay=3                                                                   
bootfile=uImage                                                               
consoledev=ttyS0                                                               
eth1addr=00:e0:0c:00:67:01                                                     
eth2addr=00:e0:0c:00:67:02                                                     
eth3addr=00:e0:0c:00:67:03                                                     
eth4addr=00:e0:0c:00:67:04                                                     
eth5addr=00:e0:0c:00:67:05                                                     
eth6addr=00:e0:0c:00:67:06                                                     
eth7addr=00:e0:0c:00:67:07                                                     
eth8addr=00:e0:0c:00:67:09                                                     
eth9addr=00:e0:0c:00:67:09                                                     
ethact=FM1@DTSEC2                                                             
ethaddr=00:e0:0c:00:67:00                                                     
ethprime=FM1@DTSEC2                                                           
fdtaddr=c00000                                                                 
fdtfile=uImage-p4080ds.dtb                                                     
fman_ucode=eff00000                                                           
gatewayip=192.168.1.1                                                         
hvboot=setenv bootargs console=ttyS0,115200 config-addr=0xfe8900000;bootm 0xfe87
00000 - 0xfe8800000                                                           
hwconfig=fsl_ddr:ctlr_intlv=cacheline,bank_intlv=cs0_cs1;fsl_fm1_xaui_phy:xfi;fs
l_fm2_xaui_phy:xfi                                                             
ipaddr=192.168.1.103                                                           
loadaddr=1000000                                                               
netdev=eth0                                                                   
netmask=255.255.255.0                                                         
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:
$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrat
e $othbootargs;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr -
$fdtaddr                                                                     
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othboota
rgs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfi
le;bootm $loadaddr $ramdiskaddr $fdtaddr                                       
ramdiskaddr=2000000                                                           
ramdiskfile=fsl-image-flash-p4080ds.ext2.gz.u-boot                             
rootpath=/opt/nfsroot                                                         
sataboot=setenv bootargs root=/dev/sda1 rootdelay=5 rw console=$consoledev,$baud
rate $othbootargs;bootm e8020000 - e8800000                                   
serverip=192.168.1.101                                                         
stderr=serial                                                                 
stdin=serial                                                                   
stdout=serial                                                                 
tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && eras
e $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize && protect on $ub
ootaddr +$filesize && cmp.b $loadaddr $ubootaddr $filesize                     
uboot=u-boot-P4080DS.bin                                                       
ubootaddr=0xeff80000                                                           
                                                                               
Environment size: 1909/8188 bytes

And attached is what I did for hypervisor deployment.

Thanks & Regards,

Peter

0 项奖励
回复

5,327 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Peter,

It reports the error "image size exceeds target window", please check whether you flashes uImage at the correct bank. Probably it's better to begin with the default two partitions hypervisor configuration  to verify the environment setup.

Thanks,

Yiping

0 项奖励
回复

5,327 次查看
peterzheng
Contributor II

Hi Yiping,

Thank you for your reply. I have deployed the hypervisor at the alternative bank, would this be the issue? Also, for uImage, I have choose the following file, is this correct?

/build/tmp/deploy/images/uImage

Regards,

Peter

0 项奖励
回复