Connecting the T1040 to the P1011 via PCIe.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting the T1040 to the P1011 via PCIe.

481 Views
darrellblock
NXP Employee
NXP Employee

We have a customer looking to establish communication on the T1040 and P1011 via PCIe.  These boards will start up independently and either one could reset without resetting the other.  They are looking for information on the behavior of the PCIe controller in the error conditions.  Scenarios they are concerned with are: 

  1. Exactly what happens on a processor if it tries to talk to the other processor which is held in reset.
  2. Exactly what happens on a processor if it tries to talk to the other processor which is powered but has not yet configured the PCIe controller. 
  3. What could happen if processor A is in the process of communicating with processor B when processor B resets
Labels (1)
0 Kudos
1 Reply

330 Views
Pavel
NXP Employee
NXP Employee

If processor is in reset state or PCI controller is not initialized or disable, this processor does not have possibility for PCI communications. It will ignore all transaction or request from PCI bus.

Look at the following pages:

http://www.design-reuse.com/articles/15545/integrating-pci-express-ip-in-a-soc.html

http://unix.stackexchange.com/questions/73908/how-to-reset-cycle-power-to-a-pcie-device

http://unix.stackexchange.com/questions/29775/reset-a-pci-device-in-linux


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos