Hi,
I'm using the QorIQ sdk 1.6 and successfully created the 'fsl-image-core' files. In u-boot code we found that CONFIG_SYS_LINUX_LOWMEM_MAX_SIZE is set to
768MB hence "if (size < bootm_size)" condition becomes true and u-boot throw "WARNING: adjusting available memory to 30000000" message on console. Our DDR size is 2G. Is this warning makes sense ??
Here is the boot log:
WARNING: adjusting available memory to 30000000
## Booting kernel from Legacy Image at 01000000 ...
Image Name: Linux-3.12.19-rt30-QorIQ-SDK-V1.
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 4195156 Bytes = 4 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 02000000 ...
Image Name: fsl-image-core-p2020ds-201410290
Image Type: PowerPC Linux RAMDisk Image (gzip compressed)
Data Size: 25076961 Bytes = 23.9 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 00c00000
Booting using the fdt blob at 0xc00000
Uncompressing Kernel Image ... OK
Loading Ramdisk to 2e815000, end 2ffff4e1 ... OK
Loading Device Tree to 03ff9000, end 03fff9f9 ... OK
Using P2020 DS machine description
Memory CAM mapping: 256/256/256 Mb, residual: 1280Mb
Linux version 3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a (kuowei.hsu@sw3linux) (gcc version 4.8.1 (GCC) ) #1 SMP Wed Oct 29 16:49:51 CST 2014
Found initrd at 0xee815000:0xeffff4e1
CPU maps initialized for 1 thread per core
bootconsole [udbg0] enabled
setup_arch: bootmem
mpc85xx_ds_setup_arch()
MPC85xx DS board from Freescale Semiconductor
arch: exit
Zone ranges:
DMA [mem 0x00000000-0x2fffffff]
Normal empty
HighMem [mem 0x30000000-0x7fffffff]
Movable zone start for each node
Early memory node ranges
node 0: [mem 0x00000000-0x7fffffff]
MMU: Allocated 1088 bytes of context maps for 255 contexts
PERCPU: Embedded 7 pages/cpu @c1971000 s7104 r8192 d13376 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 522752
Kernel command line: root=/dev/ram rw console=,115200 cache-sram-size=0x10000
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Sorting __ex_table...
Memory: 1979676K/2097152K available (6000K kernel code, 316K rwdata, 1792K rodata, 268K init, 1217K bss, 117476K reserved, 1310712K highmem)
Kernel virtual memory layout:
* 0xfff5f000..0xfffff000 : fixmap
* 0xffc00000..0xffe00000 : highmem PTEs
* 0xffbfd000..0xffc00000 : early ioremap
* 0xf1000000..0xffbfd000 : vmalloc & ioremap
SLUB: HWalign=32, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=2.
NR_IRQS:512 nr_irqs:512 16
mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe40000, max 2 CPUs
mpic: ISU size: 256, shift: 8, mask: ff
mpic: Initializing for 256 sources
clocksource: timebase mult[d555555] shift[24] registered
Console: colour dummy device 80x25
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
mpic: requesting IPIs...
Brought up 2 CPUs
devtmpfs: initialized
NET: Registered protocol family 16
Found FSL PCI host bridge at 0x00000000ffe0a000. Firmware bus number: 0->1
PCI host bridge /pcie@ffe0a000 (primary) ranges:
MEM 0x00000000c0000000..0x00000000dfffffff -> 0x00000000c0000000
IO 0x00000000ffc20000..0x00000000ffc2ffff -> 0x0000000000000000
/pcie@ffe0a000: PCICSRBAR @ 0xfff00000
PCI: Probing PCI hardware
fsl-pci ffe0a000.pcie: PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
pci_bus 0000:00: root bus resource [mem 0xc0000000-0xdfffffff]
pci_bus 0000:00: root bus resource [bus 00-ff]
pci 0000:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)
pci 0000:00:00.0: PCI bridge to [bus 01-ff]
pci 0000:00:00.0: PCI bridge to [bus 01]
pci 0000:00:00.0: bridge window [io 0x0000-0xffff]
pci 0000:00:00.0: bridge window [mem 0xc0000000-0xdfffffff]
fsl-l2ctlr ffe20000.l2-cache-controller: Entire L2 as cache, provide valid sram address and size
fsl-l2ctlr: probe of ffe20000.l2-cache-controller failed with error -22
bio: create slab <bio-0> at 0
Freescale Elo series DMA driver
fsl-elo-dma ffe0c300.dma: #0 (fsl,eloplus-dma-channel), irq 76
fsl-elo-dma ffe0c300.dma: #1 (fsl,eloplus-dma-channel), irq 77
fsl-elo-dma ffe0c300.dma: #2 (fsl,eloplus-dma-channel), irq 78
fsl-elo-dma ffe0c300.dma: #3 (fsl,eloplus-dma-channel), irq 79
fsl-elo-dma ffe21300.dma: #0 (fsl,eloplus-dma-channel), irq 20
fsl-elo-dma ffe21300.dma: #1 (fsl,eloplus-dma-channel), irq 21
fsl-elo-dma ffe21300.dma: #2 (fsl,eloplus-dma-channel), irq 22
fsl-elo-dma ffe21300.dma: #3 (fsl,eloplus-dma-channel), irq 23
Thanks for all your help in community.
Regards,
Hsu
Solved! Go to Solution.
Hello Kuowei,
It makes sense, because for PowerPC arch the Linux low memory size is configured as 0x30000000(768M), you also could get the configuration "CONFIG_LOWMEM_SIZE=0x30000000" in Linux Kernel configuration file.
Linux OS divides its virtual address space into two regions, the larger is used for user space and the smaller is for Kernel.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Kuowei,
It makes sense, because for PowerPC arch the Linux low memory size is configured as 0x30000000(768M), you also could get the configuration "CONFIG_LOWMEM_SIZE=0x30000000" in Linux Kernel configuration file.
Linux OS divides its virtual address space into two regions, the larger is used for user space and the smaller is for Kernel.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------