Booting kernel issue, hang on "turn off boot console udbg0"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting kernel issue, hang on "turn off boot console udbg0"

Jump to solution
5,205 Views
kuoweihsu
Contributor III

Hi,

I using SDK1.6, cpu base p2020 for our costumized board which built "fsl-image-core".

Our uboot file, uImage file, file system and dtb file were all from SDK1.6.


Here are what we setting in u-boot


"consoledev=ttyS0"

"console=$consoledev,$baudrate $othbootargs;"

Here is the boot log:


WARNING: adjusting available memory to 30000000

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   Linux-3.12.19-rt30-QorIQ-SDK-V1.

   Image Type:   PowerPC Linux Kernel Image (gzip compressed)

   Data Size:    4167996 Bytes = 4 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 02000000 ...

   Image Name:   fsl-image-core-p2020rdb-20141031

   Image Type:   PowerPC Linux RAMDisk Image (gzip compressed)

   Data Size:    25076593 Bytes = 23.9 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 00c00000

   Booting using the fdt blob at 0xc00000

   Uncompressing Kernel Image ... OK

   Loading Ramdisk to 2e815000, end 2ffff371 ... OK

   Loading Device Tree to 03ff9000, end 03fff64a ... OK

Using P2020RDB-PC machine description

Memory CAM mapping: 256/256/256 Mb, residual: 1280Mb

Linux version 3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a (kuowei.hsu@sw3linux) (gcc version 4.8.1 (GCC) ) #2 SMP Tue Nov 4 14:33:50 CST 2014

Found initrd at 0xee815000:0xeffff371

CPU maps initialized for 1 thread per core

bootconsole [udbg0] enabled

setup_arch: bootmem

mpc85xx_rdb_setup_arch()

mpc85xx_qe_init: Could not find Quicc Engine node

MPC85xx RDB board from Freescale Semiconductor

arch: exit

Zone ranges:

  DMA      [mem 0x00000000-0x2fffffff]

  Normal   empty

  HighMem  [mem 0x30000000-0x7fffffff]

Movable zone start for each node

Early memory node ranges

  node   0: [mem 0x00000000-0x7fffffff]

MMU: Allocated 1088 bytes of context maps for 255 contexts

PERCPU: Embedded 7 pages/cpu @c1965000 s7104 r8192 d13376 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 522752

Kernel command line: root=/dev/ram rw console=,115200 cache-sram-size=0x10000

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Sorting __ex_table...

Memory: 1979724K/2097152K available (5956K kernel code, 320K rwdata, 1784K rodata, 268K init, 1217K bss, 117428K reserved, 1310712K highmem)

Kernel virtual memory layout:

  * 0xfff5f000..0xfffff000  : fixmap

  * 0xffc00000..0xffe00000  : highmem PTEs

  * 0xffbfc000..0xffc00000  : early ioremap

  * 0xf1000000..0xffbfc000  : vmalloc & ioremap

SLUB: HWalign=32, Order=0-3, MinObjects=0, CPUs=2, Nodes=1

Hierarchical RCU implementation.

  RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=2.

NR_IRQS:512 nr_irqs:512 16

mpic: Setting up MPIC " OpenPIC  " version 1.2 at ffe40000, max 2 CPUs

mpic: ISU size: 256, shift: 8, mask: ff

mpic: Initializing for 256 sources

mpc85xx_rdb_pic_init: Could not find qe-ic node

clocksource: timebase mult[d555555] shift[24] registered

Console: colour dummy device 80x25

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

mpic: requesting IPIs...

Brought up 2 CPUs

devtmpfs: initialized

NET: Registered protocol family 16

            

Found FSL PCI host bridge at 0x00000000ffe0a000. Firmware bus number: 0->1

PCI host bridge /pcie@ffe0a000 (primary) ranges:

MEM 0x0000000080000000..0x000000009fffffff -> 0x0000000080000000

  IO 0x00000000ffc00000..0x00000000ffc0ffff -> 0x0000000000000000

/pcie@ffe0a000: PCICSRBAR @ 0xfff00000

PCI: Probing PCI hardware

fsl-pci ffe0a000.pcie: PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource [io  0x0000-0xffff]

pci_bus 0000:00: root bus resource [mem 0x80000000-0x9fffffff]

pci_bus 0000:00: root bus resource [bus 00-ff]

pci 0000:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)

pci 0000:00:00.0: PCI bridge to [bus 01-ff]

PCI: Cannot allocate resource region 0 of device 0000:01:00.0, will remap

pci 0000:01:00.0: BAR 0: assigned [mem 0x80000000-0x8003ffff 64bit]

pci 0000:00:00.0: PCI bridge to [bus 01]

pci 0000:00:00.0:   bridge window [io  0x0000-0xffff]

pci 0000:00:00.0:   bridge window [mem 0x80000000-0x9fffffff]

fsl-l2ctlr ffe20000.l2-cache-controller: Entire L2 as cache, provide valid sram address and size

fsl-l2ctlr: probe of ffe20000.l2-cache-controller failed with error -22

bio: create slab <bio-0> at 0

Freescale Elo series DMA driver

fsl-elo-dma ffe0c300.dma: #0 (fsl,eloplus-dma-channel), irq 76

fsl-elo-dma ffe0c300.dma: #1 (fsl,eloplus-dma-channel), irq 77

fsl-elo-dma ffe0c300.dma: #2 (fsl,eloplus-dma-channel), irq 78

fsl-elo-dma ffe0c300.dma: #3 (fsl,eloplus-dma-channel), irq 79

fsl-elo-dma ffe21300.dma: #0 (fsl,eloplus-dma-channel), irq 20

fsl-elo-dma ffe21300.dma: #1 (fsl,eloplus-dma-channel), irq 21

fsl-elo-dma ffe21300.dma: #2 (fsl,eloplus-dma-channel), irq 22

fsl-elo-dma ffe21300.dma: #3 (fsl,eloplus-dma-channel), irq 23

vgaarb: loaded

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

EDAC MC: Ver: 3.0.0

Advanced Linux Sound Architecture Driver Initialized.

Switched to clocksource timebase

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

rootfs image is not initramfs (no cpio magic); looks like an initrd

Freeing initrd memory: 24488K (ee815000 - effff000)

Freescale PMC driver

audit: initializing netlink socket (disabled)

type=2000 audit(0.304:1): initialized

bounce pool size: 64 pages

HugeTLB registered 1 MB page size, pre-allocated 0 pages

HugeTLB registered 4 MB page size, pre-allocated 0 pages

HugeTLB registered 16 MB page size, pre-allocated 0 pages

HugeTLB registered 64 MB page size, pre-allocated 0 pages

HugeTLB registered 256 MB page size, pre-allocated 0 pages

HugeTLB registered 1 GB page size, pre-allocated 0 pages

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

Installing knfsd (copyright (C) 1996 okir@monad.swb.de).

NTFS driver 2.1.30 [Flags: R/O].

jffs2: version 2.2. (NAND) ? 2001-2006 Red Hat, Inc.

msgmni has been set to 1485

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

Serial: 8250/16550 driver, 2 ports, IRQ sharing enabled

serial8250.0: ttyS0 at MMIO 0xffe04500 (irq = 42, base_baud = 37500000) is a 16550A

serial8250.0: ttyS1 at MMIO 0xffe04600 (irq = 42, base_baud = 37500000) is a 16550A

Generic non-volatile memory driver v1.1

brd: module loaded

loop: module loaded

nbd: registered device at major 43

st: Version 20101219, fixed bufsize 32768, s/g segs 256

of-flash ef000000.nor: do_map_probe() failed

fsl-lbc ffe05000.localbus: address did not match any chip selects

fsl_espi ffe07000.spi: master is unqueued, this is deprecated

m25p80 spi32766.0: found mr25h256, expected m25p80

m25p80 spi32766.0: mr25h256 (32 Kbytes)

5 ofpart partitions found on MTD device spiffe07000.0

Creating 5 MTD partitions on "spiffe07000.0":

0x000000000000-0x000000100000 : "SPI U-Boot Image"

mtd: partition "SPI U-Boot Image" extends beyond the end of device "spiffe07000.0" -- size truncated to 0x8000

ftl_cs: FTL header not found.

0x000000100000-0x000000180000 : "SPI DTB Image"

mtd: partition "SPI DTB Image" is out of reach -- disabled

ftl_cs: FTL header not found.

0x000000180000-0x000000580000 : "SPI Linux Kernel Image"

mtd: partition "SPI Linux Kernel Image" is out of reach -- disabled

ftl_cs: FTL header not found.

0x000000580000-0x000000980000 : "SPI Compressed RFS Image"

mtd: partition "SPI Compressed RFS Image" is out of reach -- disabled

ftl_cs: FTL header not found.

0x000000980000-0x000001000000 : "SPI JFFS2 RFS"

mtd: partition "SPI JFFS2 RFS" is out of reach -- disabled

ftl_cs: FTL header not found.

fsl_espi ffe07000.spi: at 0xf10a6000 (irq = 59)

libphy: Fixed MDIO Bus: probed

libphy: Freescale PowerQUICC MII Bus: probed

libphy: Freescale PowerQUICC MII Bus: probed

fsl-gianfar ffe24000.ethernet: enabled errata workarounds, flags: 0x4

fsl-gianfar ffe24000.ethernet eth0: mac: 00:e0:0c:02:00:fd

fsl-gianfar ffe24000.ethernet eth0: Running with NAPI enabled

fsl-gianfar ffe24000.ethernet eth0: RX BD ring size for Q[0]: 256

fsl-gianfar ffe24000.ethernet eth0: TX BD ring size for Q[0]: 256

fsl-gianfar ffe25000.ethernet: enabled errata workarounds, flags: 0x4

fsl-gianfar ffe25000.ethernet eth1: mac: 00:e0:0c:02:01:fd

fsl-gianfar ffe25000.ethernet eth1: Running with NAPI enabled

fsl-gianfar ffe25000.ethernet eth1: RX BD ring size for Q[0]: 256

fsl-gianfar ffe25000.ethernet eth1: TX BD ring size for Q[0]: 256

fsl-gianfar ffe26000.ethernet: enabled errata workarounds, flags: 0x4

fsl-gianfar ffe26000.ethernet eth2: mac: 00:e0:0c:02:02:fd

fsl-gianfar ffe26000.ethernet eth2: Running with NAPI enabled

fsl-gianfar ffe26000.ethernet eth2: RX BD ring size for Q[0]: 256

fsl-gianfar ffe26000.ethernet eth2: TX BD ring size for Q[0]: 256

pps pps0: new PPS source ptp0

ucc_geth_driver: QE UCC Gigabit Ethernet Controller

e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k

e1000e: Copyright(c) 1999 - 2013 Intel Corporation.

ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver

ohci-pci: OHCI PCI platform driver

usbcore: registered new interface driver usb-storage

i2c /dev entries driver

mpc-i2c ffe03000.i2c: timeout 1000000 us

mpc-i2c ffe03100.i2c: timeout 1000000 us

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

/soc@ffe00000/sdhc@2e000: voltage-ranges unspecified

mmc0: SDHCI controller on ffe2e000.sdhc [ffe2e000.sdhc] using DMA

talitos ffe30000.crypto: hwrng

talitos ffe30000.crypto: max_xor_srcs 6

talitos ffe30000.crypto: fsl,sec3.1 algorithms registered in /proc/crypto

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

snd-soc-p1022ds: missing/invalid global utils node

ipip: IPv4 over IPv4 tunneling driver

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

NET: Registered protocol family 15

Key type dns_resolver registered

turn off boot console udbg0

==No more log .........================

Q1. Is message "turn off boot console udbg0" is correct behavior??? Why no more messages after that??

Q2. Our setting for console is ttyS0, why it changes to udbg0 ???

Q2. If this message is right, how should I configure more to see following message ?? Example, turn on ??

Thanks for all your help in community.


Regards,

Hsu

Labels (1)
0 Kudos
Reply
1 Solution
2,845 Views
kuoweihsu
Contributor III

Hi, All,

The $consoledev is not set. Set it into ttyS0 and this problem will fixed! Thanks a lot!!!

View solution in original post

0 Kudos
Reply
3 Replies
2,845 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Kuowei,

Have you noticed that in your boot log the line "Kernel command line: root=/dev/ram rw console=,115200 cache-sram-size=0x10000" is printed? It means "ttyS0" is not passed to "console".

Here is an example, please have a reference.

=> pri ramboot

ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdtaddr

=> pri consoledev

consoledev=ttyS0

If you problem remains, please provide you u-boot environment variables with "pri" command.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,845 Views
kuoweihsu
Contributor III

Dear Yiping,

Yes, we found that the u-boot configuration is much older and the variable $consoledev is not set. We make a mistake and give the root cause for somebody meet the same error. Thanks for your example, it is useful.

0 Kudos
Reply
2,846 Views
kuoweihsu
Contributor III

Hi, All,

The $consoledev is not set. Set it into ttyS0 and this problem will fixed! Thanks a lot!!!

0 Kudos
Reply