P2040/P2041 Local Bus Specific FAQs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2040/P2041 Local Bus Specific FAQs

P2040/P2041 Local Bus Specific FAQs

Can you please give more details about 32 address signals for the eLBC implementation on P2040?

Below is a detailed explanation of 32 address signals for the eLBC implementation on P2040:

LAD[0:15] - these are multiplexed address/data signals that need to be externally latched using the LALE signal.

LA[16:31] - these are dedicated address signals.

LAD[0] is the most significant address signal and LA[31] is the least significant address signal.


Can the Local Bus FCM support two, 2GByte (16Gbit) NAND devices, if they are the appropriate page size (2K SLC)?

FCM can support two devices, each one is connected to a separate /CS.


Labels (1)
Comments

> LAD[0] is the most significant address signal and LA[31] is the least significant address signal.

I am working on P2020 design. Is above description the same for P2020?

(and I am wondering why most significant address signal is indexed as 0)

And can you clarify correspondence between LWE#0/LWE#1 and LAD[0:7]/LAD[8:15]?


Yes, it's the same for P2020. According to figure 12-33 in P2020RM.pdf LWE0 is for LAD[0:7].

Thank you, Liang-san.

No ratings
Version history
Last update:
‎08-06-2012 10:10 AM
Updated by: