P1024/P1015 Clocking Specific FAQs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1024/P1015 Clocking Specific FAQs

P1024/P1015 Clocking Specific FAQs

For P1015, does DDRCLK and PCIe (SerDes) ref clock support a spread spectrum reference?

DDRCLK and PCIe (SerDes) ref clock support spread spectrum. Please note that since SGMII doesn't support spread spectrum, if SGMII is used on any SERDES lane, spread spectrum should not be applied to SERDES REF clock.


What are the DDRCLK and PCIe (SerDes) reference clock spread spectrum parameters for P1015? 

DDRCLK and PCIe (SerDes) reference clock are designed to work with a spread spectrum clock (+0 to –0.5% spreading at 30–33 KHz rate is allowed), assuming both ends have same reference clock. For better results, a source without significant unintended modulation should be used.


标签 (1)
无评分
版本历史
最后更新:
‎08-06-2012 09:24 AM
更新人: