P1020/P1011 Hardware Specifications/Reference Manual Specific FAQs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1020/P1011 Hardware Specifications/Reference Manual Specific FAQs

P1020/P1011 Hardware Specifications/Reference Manual Specific FAQs

If unused, how do I terminate following pins in P1011/P1020: SDHC_DATA[0:2], SDHC_DAT3, SPI_CS[0:3]/SDHC_DAT[4:7] and SPI_CS0_B/SDHC_DATA4?

All the 3 pins SDHC_DATA[0:2], SDHC_DAT3 and SPI_CS[0:3]/SDHC_DAT[4:7] should be don't care if not used. Please leave SPI_CS0_B.SDHC_DATA4 as floating when not used.


I have designed my P1011 board based on the older hardware spec, and found that AVDD_CORE0 and AVDD_CORE1 were swapped in newer hardware spec. At this time, it is difficult to cut the pattern for the current AVDD_CORE1. So 1.0V power applied to AVDD_CORE1 though core 1 is not used. Does this cause any problem?

If AVDD_CORE1 is powered in single core device, there'll be no problem. But if AVDD_CORE0 is not powered in single core device, the device may not boot up.


How should I handle pin W26,F16 pins in P1020? Just let them "NC", or need connect them to AVdd?

If AVDD_CORE1 is not powered up i.e. connected to 1.0V, the single core p101x device cannot be boot up. Please implement the AVDD circuit at this stage.


标签 (1)
无评分
版本历史
最后更新:
‎07-25-2012 10:33 AM
更新人: