P1020/P1011 Clocking Specific FAQs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1020/P1011 Clocking Specific FAQs

P1020/P1011 Clocking Specific FAQs

Can you give detailed information about P1011/20 clock in sources - SYSCLK, DDCCLK and eTSEC_Clock_125? Do these CLOCK source in support Spread Spectrum? What about SD_REF_CLK/SD_REF_CLK#?

The spread spectrum parameters table in P1020 HW Spec is valid for SYSCLK and DDRCLK.

Spread spectrum clock is not supported for EC_GTX_CLK125 (RGMII).

For SERDES, SD_REF_CLK/SD_REF_CLK_B are designed to work with a spread spectrum clock (+0 to –0.5% spreading at 30–33 KHz rate is allowed), assuming both ends have same reference clock. For better results, a source without significant unintended modulation should be used.

Please note that since SGMII doesn't support spread spectrum, if SGMII is used on any SERDES lane, spread spectrum should not be applied to SERDES REF Clock.


标签 (1)
无评分
版本历史
最后更新:
‎07-25-2012 10:37 AM
更新人: