Enabling SD Interface on P1010 Reference Design Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enabling SD Interface on P1010 Reference Design Board

Enabling SD Interface on P1010 Reference Design Board

To enable SD interface in SPI boot on P1010RDB: 1. Perform the following updates in u-boot a) Modify pmuxcr to enable SD bus in case of SPI boot b) Update the corresponding static mux implementation in u-boot 2. Perform the following updates in Linux a) Disable IFC from device tree and kernel defconfig

The patch details to enable SD interface are given below. A zip file, AN4336SW.zip, containing the patches for u-boot and Linux accompanies this application note. The file can be downloaded from [1].

U-Boot

  •   Extract the u-boot code from the QorIQ SDK 1.0.1 iso
  •   Apply the patch, u-boot-p1010rdb-enabling-sd-in-spi-boot.patch
  •   Compile the u-boot using "make" command for SPI Flash
   make ARCH=powerpc   CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.5.55-eglibc-2.11.55/powerpc-linux-gnu/bin/powerpc-linux-gnu- P1010RDB_SPIFLASH
  •   Use the boot_format utility to generate the spiimage. For more information, see SDK manual.
  •   Update the SPI Flash with the above built spiimage

Linux

  • Extract the Linux source code from QorIQ SDK 1.0.1 iso
  • Apply the patch, linux-p1010rdb-enabling-sd-in-spi-boot.patch
  • Compile Linux using make command
 #make ARCH=powerpc  CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.5.55-eglibc-2.11.55/powerpc-linux-gnu/bin/powerpc-linux-gnuarch/  powerpc/configs/qoriq_sdk_nonsmp_defconfig  #make ARCH=powerpc  CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.5.55-eglibc-2.11.55/powerpc-linux-gnu/bin/powerpc-linux-gnu-
  • Compile the dts
 ./sripts/dtc/dtc -f -I dts -O dtb -R 8 -S 0x3000  arc/powerpc/boot/dts/p1010rdb.dts.dts > p1010rdb.dtb.dtb
  • With the updated SPI bootloader, Linux uImage and p1010rdb.dtb, the user must be able to enable SD interface on P1010RDB.


NOTE

  • The above-mentioned changes must be done only when the user specifically requires the SD interface using SPI boot.
  • For all other boot methods, these patches must not be used.


标签 (1)
评论

Hello!

Is it possible to enable SD Interface with IFC boot?

The current BSP seems to disable it by default.

Tks,

Bruno

无评分
版本历史
最后更新:
‎09-10-2020 01:52 AM
更新人: