writing Mifare classic 1k card using OM26630FDK AND NXP NFC COCKPIT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

writing Mifare classic 1k card using OM26630FDK AND NXP NFC COCKPIT

821 次查看
suhas_badve1
Contributor I

Hi 

We are using OM26630FDK AND NXP NFC COCKPIT to evaluate CLRC663 Plus chip.

We are able to check UID if Mifare cliassic 1k card using the kit and NFC cockpit software.

now we want to read Mifare classic 1K card E2prom and write in the Mifare classic 1K card.

but we are not getting any sequece or procedure to follow to read /write in Mifare classic card using 

OM26630FDK AND NXP NFC COCKPIT. Please guide us and share the steps.

 

Thanks

0 项奖励
回复
6 回复数

794 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @suhas_badve1

Hope you are doing well.

Please, consider that MIFARE Classic EV1 1K - 4K is not recommended for new designs. Instead, we recommend using our MIFARE® DESFire® Light IC.

Supported operations in NFC Cockpit are described in the NXP NFC Cockpit User Guide.

For Read/Write operations using MIFARE Classis, please consider using the NFC Reader Library. This library provides an API that facilitates the most common operations required in NFC applications such as reading or writing data. It includes an example of the implementation of MIFARE Classic.

Regards,
Eduardo.

0 项奖励
回复

781 次查看
suhas_badve1
Contributor I
Hi ,

How can we initiate reading /writing data in mifare classic card from NXP NFC cockpit. I understood how we check UID, but unable to understand how we can write data in Card ot read data from card using nxp NFC cockpit utility.
0 项奖励
回复

712 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Perhaps you could use the Data Exchange as illustrated in the NXP NFC Cockpit User Guide, Figure 43. However, there may not be any document or guide that could meet your requirements, this data exchange should be based on the commands from ISO/IEC 14443 Type-A.

Additionally, I would recommend you taking a look at the RFIDDiscover software. This tool can be used for MIFARE devices and allows to access and handle any MIFARE family chip and data processing feature.

I apologize for any inconvenience this might cause you.

Regards,
Eduardo.

0 项奖励
回复

690 次查看
suhas_badve1
Contributor I
Thanks for the input.
Does RFID Discover software works with OM26630FDK.
We have this board so that we can test the app with this kit
0 项奖励
回复

672 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

You can find the supported readers in the RFIDDiscover product page. Please notice that there might be some differences depending on the software version (Lite/Full).

Regards,
Eduardo.

0 项奖励
回复

366 次查看
suhas_badve1
Contributor I
Hi,
I am using CLEV6630B board for RFID reader and want to read/write on Mifare classic card.

I am using NFCrdlibEx4_Mifareclassic library code. I want to add UART communication in this code so that I can connect the board to PC over serial and send the card information to PC. 

I want to develop PC based software through which I can send the commands to the CLEV6630B board to write some data in the Mifare Classic card, read data from Mifare Classic card etc. In short I want to add UART interface on TXD0 and RXD0 (which is available on CLEV6630B) in NFCrdlibEx4_Mifareclassic code

Please guide. Please share some sample code.

Thanks.
0 项奖励
回复