would you like kindly help to recommend the Operation Amplifier for our new project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

would you like kindly help to recommend the Operation Amplifier for our new project

Jump to solution
814 Views
Guofred
Contributor III

Hi,

i couldn't find the operation amplifier  on the NXP website. 

the operation amplifier requirement as below:

->Channel:  single channel

->VCC:  12V max

->output short current Isc : < 500 mA max, <=200mA is accept

->temperature:  -40~125℃

->Slew rate:   50V/uS

->Package: SOT-23-5

-> Application:  Automotive

only find some amplifier such as used in Audio-(Class D and Class AB ), Radio amplifier etc ,

they are not to meet the requirement, would you like kindly help to recommend some NXP amplifier or

share your comments, thanks.

Best regards.

Guofred

0 Kudos
Reply
1 Solution
795 Views
guoweisun
NXP TechSupport
NXP TechSupport

 All of the Automotive PA focus on high power, you can get all of them below link:

Car Audio Amplifiers | NXP Semiconductors

View solution in original post

0 Kudos
Reply
2 Replies
796 Views
guoweisun
NXP TechSupport
NXP TechSupport

 All of the Automotive PA focus on high power, you can get all of them below link:

Car Audio Amplifiers | NXP Semiconductors

0 Kudos
Reply
785 Views
Guofred
Contributor III

Hi @guoweisun ,

Thanks for your kindly help.

i would like to check it again, thanks.

 

Best regards.

Guofred

0 Kudos
Reply