why MRFE6VS25GN device model is not working AWR simulation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why MRFE6VS25GN device model is not working AWR simulation?

2,492 Views
raveendrareddy
Contributor II

Hi, 

I would like to simulate MRFE6VS25GN device in NI AWR software and found that it is not working and seems it is problem with model which is provided by NXP, in the design kit i didn't find any Model64 folder.

Would you please help us to provide correct simulation model for AWR?

Also it would be great help to provide any document which has input and output impedance in the frequency band of 960-1215 MHz.

Labels (1)
  • RF

Tags (1)
5 Replies

2,415 Views
LPP
NXP Employee
NXP Employee


Please, I sent you a model kit that includes 64-bit version.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,415 Views
raveendrareddy
Contributor II

Thanks for the response. I didn't receive the model in the email, would you please send the email or send link to download the model.

0 Kudos
Reply

2,415 Views
LPP
NXP Employee
NXP Employee


I created a new support ticket #00285164 and sent a mail to you.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,415 Views
raveendrareddy
Contributor II

Hi Pavel,

May I know the link for support ticket and I didn't receive any mail to address this issue, and today i received email that our NXP support case: #00285164 is closed.

Would you please help me to provide model for this?

0 Kudos
Reply

2,415 Views
LPP
NXP Employee
NXP Employee

The problem is solved.

Pavel