what does MC33908 work if input voltage range higher than 28V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what does MC33908 work if input voltage range higher than 28V

657 Views
xin_zhao
Contributor I

Hello,

I want use MC33908 for 24v System, but I found its green operation voltage range was 6.0~28V. The max voltage in 24V system may higher than 28V. In datasheet it is said between 28V~40V " Potential Vpre thermal limitation". What will MC33908 works between 28V to 40V? If my load is not high, can I use it in 24V system?

Tags (1)
0 Kudos
1 Reply

587 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

Our proposal for 24V systems, as shown in Figure 31 of AN4766, is to insert a Maxim device MAX6495 between Vbat and Vsup to protect the input voltage of MC33908, plus other local protections on pins going or coming from outside of the module.

Best regards,

Tomas

0 Kudos