Hello NXP support team,
Build configuration
ubuntu 18.04
MACHINE=imx6qdlsabresd DISTRO=fsl-imx-wayland source ./imx-setup-release.sh -b build
bitbake core-image-base
Build Configuration:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qdlsabresd"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "5.15-kirkstone"
TUNE_FEATURES = "arm vfp cortexa9 neon thumb callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:27de52e402ae000dfa502d52908cd6e6aef923ec"
meta-oe
meta-multimedia
meta-python = "HEAD:5357c7a40eaf8d1bcf7ff58edbba8e9527e40c7d"
meta-freescale = "HEAD:2fb1ce365338126aad365012ebb913b3e4a9f1be"
meta-freescale-3rdparty = "HEAD:de0eb1408150d77f9cce97c559f9a5a3c71e5d6c"
meta-freescale-distro = "HEAD:fc15f5003043da23212596be7366ae2547c308ad"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:5bc708f56575a878da17f2148e959c95d06cf8db"
meta-nxp-demo-experience = "HEAD:8fade3993b832ecd823771644f2a7b731f8f4527"
meta-chromium = "HEAD:d25d8ee98a656b2534d0eec6138ef264529fab4f"
meta-clang = "HEAD:85d956d95401479ca666139e31f662f60c156d5f"
meta-gnome
meta-networking
meta-filesystems = "HEAD:5357c7a40eaf8d1bcf7ff58edbba8e9527e40c7d"
meta-qt6 = "HEAD:b2894aad5c1aaa85f2f5c7b94391b7c51c39e555"
meta-virtualization = "HEAD:973c8d0964c6f40338857efe5b8009b2f647d485"
Warning message
warning: you have included the meta-virtualization layer, but 'virtualization' has not been enabled in your distro_features. some bbappend files may not take effect. see the meta-virtualization readme for details on enabling virtualization support.
followed the instruction provided in i.MX Yocto Project users guide Rev. LF5.15.32_2.0.0
can you suggest how to solve the warning?
i have already verified the https://github.com/lgirdk/meta-virtualization/blob/master/README
and added the line DISTRO_FEATURES:append = " virtualization" in the below given path
meta-virtualization/blob/master/conf/layer.conf
warning not solved.
thanks
Solved! Go to Solution.
ok please close this thread
added DISTRO_FEATURES:append = " virtualization"
/meta-virtualization/blob/master/conf/layer.conf
But the warning not solved.
https://github.com/lgirdk/meta-virtualization/blob/master/README.
read the file, can you suggest path of the file
DISTRO_FEATURES:append = " virtualization"
to add the above variable