sja1110-evm connect error by usb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sja1110-evm connect error by usb

299 Views
liu8232303
Contributor I

i read device ID of SJA1110-EVM by usb,but read 0xFFFFFFFF,and led of board is red,i dont know  why?

--------------------------------------------------------------------------------------------------------------------------------------

D:\LLL\sja1110-evm\SJA1110-EVM-Host-Tools\venv\Scripts\python.exe D:\LLL\sja1110-evm\SJA1110-EVM-Host-Tools\sja1110evm_hosttools_v1.2\SJA1110EVM\read_deviceid.py
serial_numbers: [
{'index': 0, 'flags': 1, 'type': 3, 'id': 0, 'location': 0, 'serial': b'', 'description': b'', 'handle': c_void_p(None)},
{'index': 1, 'flags': 2, 'type': 7, 'id': 67330065, 'location': 8977, 'serial': b'A', 'description': b'Quad RS232-HS A', 'handle': c_void_p(None)},
{'index': 2, 'flags': 2, 'type': 7, 'id': 67330065, 'location': 8980, 'serial': b'D', 'description': b'Quad RS232-HS D', 'handle': c_void_p(None)},
{'index': 3, 'flags': 2, 'type': 7, 'id': 67330065, 'location': 8978, 'serial': b'B', 'description': b'Quad RS232-HS B', 'handle': c_void_p(None)}]
DeviceId SW1: 0xFFFFFFFF
DeviceId SW2: 0xFFFFFFFF

Process finished with exit code 0111.png

0 Kudos
Reply
1 Reply

278 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

could you try below DIP switch settings and then power off and on and then try again?

PetrS_0-1686830811551.png

BR, Petr

0 Kudos
Reply