" `FSL_AFIC10275N_FET2.FSL1' is an instance of an undefined model `FET2M1' " error in ADS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

" `FSL_AFIC10275N_FET2.FSL1' is an instance of an undefined model `FET2M1' " error in ADS

Jump to solution
2,979 Views
MohMor
Contributor III

hello, my problem is related to AFIC10275N. I've added available libraries to ADS and got one error. I have attached the error text file. I also have attached the image of my schematic below. what is my problem?

Labels (1)
  • RF

0 Kudos
1 Solution
2,636 Views
MohMor
Contributor III
3 Replies
2,637 Views
MohMor
Contributor III

Hi guys

here is the solution:

https://www.youtube.com/watch?v=UrvMeU0AwM4

best regards

2,970 Views
LPP
NXP Employee
NXP Employee

Please, check that your design includes RF_Power_ADS_DesignKit

LPP_0-1645023145693.png

Best Regards

Pavel

NXP CAS

Tags (1)
2,950 Views
MohMor
Contributor III

hi again,
when I want to add AFIC10275N_Level1_Rev0_DK a message come up. but anyway, the component exists in the schematic. I've uploaded the image of error. moreover, my design has RF_Power_ADS_DesignKit.

0 Kudos